STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Not able to update internal RTC in STM32F373

Hi,           I made a project for only internal RTC. It worked with LSI and not with LSE. Then I integrated RTC in current project which has various other features. It is not working. I am getting zero readings.      RTC initialization, get tim...

Ralph1 by Associate
  • 1796 Views
  • 3 replies
  • 0 kudos

No device found on target ERROR

I have a STM32NUCLEOF411RE. It was working well until today. Now my pc can not recognize it. It says "No device found on target.". Also when I connect my board the processor becomes too hot in a few seconds. However, when power it with 5V it does not...

AYelb.1 by Associate
  • 2614 Views
  • 5 replies
  • 0 kudos

Issue in STANDBY Mode in stm32f746g discovery board.

Hi everyone,I am trying to implement the STANDBY mode in stm32f746g board using the system wakeup pin PI11 (user push button). The issue is that once I press the button, the controller automatically wakes up from the STANDBY mode.I have attached my c...

SGupt.7 by Associate II
  • 1746 Views
  • 2 replies
  • 0 kudos

STM32L431RCT Hard Fault on SPI at HAL library

Hi,I keep on getting hard fault on HAL_SPI_Transmit_IT.I am trying to communicate to SX1276. The circuit is designed by another experienced hardware engineer.I use the similar code on STM32L431CBT without issue.However, I face random hard fault on ST...

AKuan.1 by Associate II
  • 1877 Views
  • 3 replies
  • 0 kudos