STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Enabling and disabling CCR interrupts on a running timer.

Hello all. I am trying to set up a continuously running timer to use to set of interrupts at specific counts of the timer. So the user of this thing would say "setAlarm(n)" and at timer=n an interrupt goes off. But I also want interrupts for the ccr...

JSven.9 by Associate II
  • 4586 Views
  • 5 replies
  • 0 kudos

Hello everyone I'm a RT embedded engineer and I want to ask question about HardFault_Handler debug. I'm working on STM32G070RB, Can somebody have a good tequinqe how debug HardFault_Handler?

void HardFault_Handler(void){ /* USER CODE BEGIN HardFault_IRQn 0 */  __asm volatile  (    " tst lr, #4                        \n"    " ite eq                          \n"    " mrseq r0, msp                       \n"    " mrsne r0, psp               ...

gilramon by Associate II
  • 2917 Views
  • 8 replies
  • 0 kudos

How to recover UART RX with DMA after Frame or OverRun error.

Because of nature of my application sometimes I need to disconnect the cable for UART. In tthat case frame error is detected (sometimes noise or overrun). I would like that after reconnection of the cable UART communication comes back. After reconnec...

MAnto.2 by Associate III
  • 1056 Views
  • 0 replies
  • 1 kudos

libraries st7282 or configuration st7735 object

Good morning I have a tft st7282 with which I should view manually created images (pixel by pixel color for a thermal scanner) I would need the reference library to use functions such as FIll_Rect, Draw_line etc... where can I find it? currently I ha...

Icont.1 by Associate II
  • 808 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F030 SPI1 enable bit (CR1->SPE) is not set to 1

Hi,I am trying to interface eeprom module with STM32F0308-Disco board using CUBE IDE - HAL library. SPI communication is not working properly, I am getting random values while trying to read the Eeprom ID.While debugging the code I found that the SPE...

0693W00000GXsxMQAT.png
SSala.3 by Associate III
  • 2460 Views
  • 3 replies
  • 0 kudos

STM32G0 not works after reset

HelloI work on the stm32g0 micro. i programmed it with a simple "blinky" code.it works correctly.but when i reset it doesn't work until i program it again.can you help me?

Question about calculating i2c timing

I use stm32373c_eval board and I try to acquire and send test data by i2c communication.The max speed of usb-i2c i use is 400k and board i2c clock frequency is 72M.I downloaded the I2C_Timing_Configuration_V1.0.1.xls from st website.I try to configur...

0693W00000GXoyQQAT.png
KShen.1 by Associate II
  • 3442 Views
  • 5 replies
  • 0 kudos