2024-10-27 07:07 PM - edited 2024-10-27 07:09 PM
Is it possible to input 7S into a B-G431B-ESC1 EVM with a voltage specification that says up to 6S?
If not, if I replace some parts with a high rated voltage as below, can I input 7S into EVM?
1. Power Section, TVS diode, SMM4F26A (D20) -> SMM4F33A
2. Power Section, Capacitor, 15uF 35V (C27 to C40) -> (I will keep this.)
3. Bemf Detection & Sensor Input, Schottky diode, BAT30KFILM (D10~D15, D17~D19) -> BAT48
Thank you!
Solved! Go to Solution.
2024-10-29 07:26 PM
2024-10-29 07:37 PM
The online support home will create one case for you, then one team will answer your question.
2024-10-29 07:49 PM
Thank you.
I didn't know there was a route like this.
I will use this route as soon as my question becomes specific.
Once again, thank you for using your time to me.