2024-03-17 10:46 PM - last edited on 2025-03-20 8:17 AM by Andrew Neil
I'm using the STM32G030FP6 in standby mode with WKUP2 for wakeup and the system has a backup battery. I'm facing the following issues:
2024-03-18 6:07 AM
Hi, i don't think if i can resolve your problem but did you use the PC13 GPIO on your board ?
because on the erratasheet i found this issue:
2.2.7 PC13 signal transitions disturb LSE
Description
The PC13 port toggling disturbs the LSE clock.
Workaround
NoneQM
2024-03-19 10:34 AM
On my system, PC13 is not utilized (STM32G030FP6 doesn't have PC13), and during debugging, I've discovered that I can't enable the LSEON bit of the BDCP register during abnormal startup.
2025-03-20 8:02 AM
Hello @ZZH, I trust that your issue is resolved by now.
Your post suggests that you can successfully put the STM32G0 into Standby Mode. I have difficulties with that, and posted about it (STMG0B1RET output pin does not pull down in Standby Mode) and studied several posts, to no avail.
Not sure if you can share a code snippet? Or perhaps comment on my code? I really appreciate it.