2013-08-04 9:52 AM
I am trying to get ADC regular dual mode with external trigger on timer 1 to work. I have read a lot of posts on this forum about ADC dual mode and some on external triggering, but I still can't get it to work. When I instead use software to start ADC conversions it all works as it should. So ADC conversions are not getting triggered by the timer interrupt i suspect.
 #define ADC_DATA_BUFFER_SIZE 7200 
__IO uint32_t ADCdata[ADC_DATA_BUFFER_SIZE+160]; 
void main(void) 
{ 
ADC_IQSamplingInitialization(); 
TIMER1_Enable(); 
while(1) 
{ 
} 
} 
void ADC_IQSamplingInitialization(void) 
{ 
NVIC_DmaAdcInitialization(); 
DMA_AdcInitialization(); 
ADC_Adc1Initialization(); 
ADC_Adc2Initialization(); 
//Enable timer 1 compare as external trigger 
ADC_ExternalTrigConvCmd(ADC1, ENABLE); 
ADC_ExternalTrigConvCmd(ADC2, ENABLE); 
//Enable ADC2 
ADC_Cmd(ADC2, ENABLE); 
//Enable ADC1 
ADC_Cmd(ADC1, ENABLE); 
} 
void NVIC_DmaAdcInitialization(void) 
{ 
NVIC_InitTypeDef NVIC_InitStructure; 
//Register with Nested Vectored Interrupt Controller (NVIC). 
NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel1_IRQn; 
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0A; 
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x0A; 
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; 
//Add DMA1_Channel1_IRQn to NVIC 
NVIC_Init(&NVIC_InitStructure); 
} 
void DMA_AdcInitialization(void) 
{ 
DMA_InitTypeDef DMA_InitStructure; 
//Enable DMA1 clock 
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE); 
//Configure DMA1 CH1 
DMA_Cmd(DMA1_Channel1, DISABLE); 
DMA_DeInit(DMA1_Channel1); 
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t) ADC_DATA_REGISTER_ADDRESS; 
DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t) &ADCdata[0]; 
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC; 
DMA_InitStructure.DMA_BufferSize = ADC_DATA_BUFFER_SIZE; 
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; 
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; 
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word; 
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Word; 
DMA_InitStructure.DMA_Mode = DMA_Mode_Normal; 
DMA_InitStructure.DMA_Priority = DMA_Priority_High; 
DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; 
//Initialize DMA1 CH1 
DMA_Init(DMA1_Channel1, &DMA_InitStructure); 
//Enable DMA Transfer Complete interrupt 
DMA_ITConfig(DMA1_Channel1, DMA_IT_TC, ENABLE); 
//Enable DMA1 CH1 
DMA_Cmd(DMA1_Channel1, ENABLE); 
} 
void ADC_Adc1Initialization(void) 
{ 
GPIO_InitTypeDef GPIO_InitStructure; 
ADC_InitTypeDef ADC_InitStructure; 
//ADC clk = APB2 clk / 6 = 72MHz/6 = 12MHz. MAX 14MHz. 
RCC_ADCCLKConfig(RCC_PCLK2_Div6); 
RCC_APB2PeriphClockCmd( (RCC_APB2Periph_ADC1 | RCC_APB2Periph_GPIOC) , ENABLE); 
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; 
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; 
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN; 
GPIO_Init(GPIOC, &GPIO_InitStructure); 
ADC_Cmd(ADC1, DISABLE); 
ADC_DeInit(ADC1); 
ADC_InitStructure.ADC_Mode = ADC_Mode_RegSimult; 
ADC_InitStructure.ADC_ScanConvMode = DISABLE; 
ADC_InitStructure.ADC_ContinuousConvMode = DISABLE; 
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1; 
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; 
ADC_InitStructure.ADC_NbrOfChannel = 1; 
ADC_Init(ADC1, &ADC_InitStructure); 
ADC_RegularChannelConfig(ADC1, ADC_Channel_10, 1, ADC_SampleTime_7Cycles5); 
ADC_DMACmd(ADC1, ENABLE); 
} 
void ADC_Adc2Initialization(void) 
{ 
GPIO_InitTypeDef GPIO_InitStructure; 
ADC_InitTypeDef ADC_InitStructure; 
//ADC clk = APB2 clk / 6 = 72MHz/6 = 12MHz. MAX 14MHz. 
RCC_ADCCLKConfig(RCC_PCLK2_Div6); 
RCC_APB2PeriphClockCmd( (RCC_APB2Periph_ADC2 | RCC_APB2Periph_GPIOA) , ENABLE); 
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3; 
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; 
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN; 
GPIO_Init(GPIOA, &GPIO_InitStructure); 
ADC_Cmd(ADC2, DISABLE); 
ADC_DeInit(ADC2); 
ADC_InitStructure.ADC_Mode = ADC_Mode_RegSimult; 
ADC_InitStructure.ADC_ScanConvMode = DISABLE; 
ADC_InitStructure.ADC_ContinuousConvMode = DISABLE; 
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None; 
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; 
ADC_InitStructure.ADC_NbrOfChannel = 1; 
ADC_Init(ADC2, &ADC_InitStructure); 
ADC_RegularChannelConfig(ADC2, ADC_Channel_3, 1, ADC_SampleTime_7Cycles5); 
} 
void TIMER1_Init(void) 
{ 
NVIC_InitTypeDef NVIC_InitStructure; 
TIM_TimeBaseInitTypeDef TIM_TimeBaseInitStructure; 
TIM_OCInitTypeDef TIM_OCInitStructure; 
//Enable Timer 1 clock 
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE); 
//Base 
TIM_TimeBaseStructInit(&TIM_TimeBaseInitStructure); 
TIM_TimeBaseInitStructure.TIM_Prescaler = 0; 
TIM_TimeBaseInitStructure.TIM_CounterMode = TIM_CounterMode_Up; 
TIM_TimeBaseInitStructure.TIM_Period = 60167; 
TIM_TimeBaseInitStructure.TIM_ClockDivision = TIM_CKD_DIV1; 
TIM_TimeBaseInit(TIM1, &TIM_TimeBaseInitStructure); 
TIM_ARRPreloadConfig(TIM1, ENABLE); 
//Register with Nested Vectored Interrupt Controller (NVIC). 
NVIC_InitStructure.NVIC_IRQChannel = TIM1_CC_IRQn; 
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0B; 
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x0B; 
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; 
NVIC_Init(&NVIC_InitStructure); 
//Clear timer 
TIM_SetCounter(TIM1, 0); 
//Interrupt 
TIM_ITConfig(TIM1, TIM_IT_CC1, ENABLE); 
} 
void TIMER1_Enable(void) 
{ 
//Clear timer 
TIM_SetCounter(TIM1, 0); 
//Enable timer 
TIM_Cmd(TIM1, ENABLE); 
} 
void TIMER1_Disable(void) 
{ 
//Disable timer 
TIM_Cmd(TIM1, DISABLE); 
} 
void TIM1_CC_IRQHandler(void) 
{ 
//Clear timer 1 compare interrupt flag 
TIM_ClearITPendingBit(TIM1, TIM_IT_CC1); 
} 
void DMA1_Channel1_IRQHandler(void) 
{ 
//Clear DMA Transfer complete interrupt flag 
DMA_ClearITPendingBit(DMA1_IT_TC1); 
//Light LED2 
LED(LED2, ON); 
}    
   
  I am trying to get ADC regular dual mode with external trigger on timer 1 to work. I have read a lot of posts on this forum about ADC dual mode and some on external triggering, but I still can't get it to work. When I instead use software to start ADC conversions it all works as it should. So ADC conversions are not getting triggered by the timer interrupt i suspect.
#adc-dma-tim-dualmode2013-08-04 6:23 PM
You want to configure channel 1 settings of the timer to use it for generating a trigger.
You don't be interrupting with the high periodicity of CC1, there's no point to doing this. For TIM1 or 8 you're likely to need to enable the PWM output. For non-circular DMA you'll have to repeatedly restart it.2013-08-07 11:40 AM
You are absolutly right! I forgot to configure timer 1 channel 1 and enabling PWM output. Thank you clive1 =)