cancel
Showing results for 
Search instead for 
Did you mean: 

ADC Calibration Return Fails due to ADC_CALIBRATION_TIMEOUT on STM32G030X6

ogulcanyanik
Visitor

First of all , I read this post (https://community.st.com/t5/stm32-mcus-products/adc-calibration-doesn-t-complete-on-stm32g0c1re/td-p/590459)  that was previously opened on this subject. I think the issue is noy completly resolved because there is a misunderstanding. 

I'm using STM32Cube MCU Package for STM32G0 Series, software package.

As @Imen.D  replied on 2024-03-26 , 04:44 pm in this post (https://community.st.com/t5/stm32-mcus-products/adc-calibration-doesn-t-complete-on-stm32g0c1re/td-p/590459:(

  • In fact, the delay is required for ADC disable to be effective (therefore, applicable between ADC disable and calibration start, or between ADC disable and calibration factor set). 

I couldnt see delay placed in the relevant code sections. 

Even if I put uS delays to those sections. It didnt work. 

 

Here is the problem : 

HAL_StatusTypeDef HAL_ADCEx_Calibration_Start(ADC_HandleTypeDef *hadc)
{
HAL_StatusTypeDef tmp_hal_status;
__IO uint32_t wait_loop_index = 0UL;
uint32_t backup_setting_cfgr1;
uint32_t calibration_index;
uint32_t calibration_factor_accumulated = 0;
uint32_t tickstart;
uint32_t adc_clk_async_presc;
__IO uint32_t delay_cpu_cycles;

/* Check the parameters */
assert_param(IS_ADC_ALL_INSTANCE(hadc->Instance));

__HAL_LOCK(hadc);

/* Calibration prerequisite: ADC must be disabled. */

/* Disable the ADC (if not already disabled) */
tmp_hal_status = ADC_Disable(hadc);
delay_uS(20); // added by me
/* Check if ADC is effectively disabled */
if (LL_ADC_IsEnabled(hadc->Instance) == 0UL)
{
/* Set ADC state */
ADC_STATE_CLR_SET(hadc->State,
HAL_ADC_STATE_REG_BUSY,
HAL_ADC_STATE_BUSY_INTERNAL);

/* Manage settings impacting calibration */
/* - Disable ADC mode auto power-off */
/* - Disable ADC DMA transfer request during calibration */
/* Note: Specificity of this STM32 series: Calibration factor is */
/* available in data register and also transferred by DMA. */
/* To not insert ADC calibration factor among ADC conversion data */
/* in array variable, DMA transfer must be disabled during */
/* calibration. */
backup_setting_cfgr1 = READ_BIT(hadc->Instance->CFGR1, ADC_CFGR1_DMAEN | ADC_CFGR1_DMACFG | ADC_CFGR1_AUTOFF);
CLEAR_BIT(hadc->Instance->CFGR1, ADC_CFGR1_DMAEN | ADC_CFGR1_DMACFG | ADC_CFGR1_AUTOFF);

/* ADC calibration procedure */
/* Note: Perform an averaging of 8 calibrations for optimized accuracy */
for (calibration_index = 0UL; calibration_index < 8UL; calibration_index++)
{
/* Start ADC calibration */
LL_ADC_StartCalibration(hadc->Instance);
delay_uS(20); // added by me
/* Wait for calibration completion */
while (LL_ADC_IsCalibrationOnGoing(hadc->Instance) != 0UL)
{
wait_loop_index++;
if (wait_loop_index >= ADC_CALIBRATION_TIMEOUT)
{
/* Update ADC state machine to error */
ADC_STATE_CLR_SET(hadc->State,
HAL_ADC_STATE_BUSY_INTERNAL,
HAL_ADC_STATE_ERROR_INTERNAL);

__HAL_UNLOCK(hadc);

return HAL_ERROR; // Code always return HAL_ERROR  due to ADC_CALIBRATION_TIMEOUT
}
}

calibration_factor_accumulated += LL_ADC_GetCalibrationFactor(hadc->Instance);
}
/* Compute average */
calibration_factor_accumulated /= calibration_index;

/* Apply calibration factor (requires ADC enable and disable process) */
LL_ADC_Enable(hadc->Instance);

/* Case of ADC clocked at low frequency: Delay required between ADC enable and disable actions */
if (LL_ADC_GetClock(hadc->Instance) == LL_ADC_CLOCK_ASYNC)
{
adc_clk_async_presc = LL_ADC_GetCommonClock(__LL_ADC_COMMON_INSTANCE(hadc->Instance));

if (adc_clk_async_presc >= LL_ADC_CLOCK_ASYNC_DIV16)
{
/* Delay loop initialization and execution */
/* Delay depends on ADC clock prescaler: Compute ADC clock asynchronous prescaler to decimal format */
delay_cpu_cycles = (1UL << ((adc_clk_async_presc >> ADC_CCR_PRESC_Pos) - 3UL));
/* Divide variable by 2 to compensate partially CPU processing cycles */
delay_cpu_cycles >>= 1UL;

while (delay_cpu_cycles != 0UL)
{
delay_cpu_cycles--;
}
}
}

LL_ADC_SetCalibrationFactor(hadc->Instance, calibration_factor_accumulated);
LL_ADC_Disable(hadc->Instance);

/* Wait for ADC effectively disabled before changing configuration */
/* Get tick count */
tickstart = HAL_GetTick();

while (LL_ADC_IsEnabled(hadc->Instance) != 0UL)
{
if ((HAL_GetTick() - tickstart) > ADC_DISABLE_TIMEOUT)
{
/* New check to avoid false timeout detection in case of preemption */
if (LL_ADC_IsEnabled(hadc->Instance) != 0UL)
{
/* Update ADC state machine to error */
SET_BIT(hadc->State, HAL_ADC_STATE_ERROR_INTERNAL);

/* Set ADC error code to ADC peripheral internal error */
SET_BIT(hadc->ErrorCode, HAL_ADC_ERROR_INTERNAL);

return HAL_ERROR;
}
}
}

/* Restore configuration after calibration */
SET_BIT(hadc->Instance->CFGR1, backup_setting_cfgr1);

/* Set ADC state */
ADC_STATE_CLR_SET(hadc->State,
HAL_ADC_STATE_BUSY_INTERNAL,
HAL_ADC_STATE_READY);
}
else
{
SET_BIT(hadc->State, HAL_ADC_STATE_ERROR_INTERNAL);

/* Note: No need to update variable "tmp_hal_status" here: already set */
/* to state "HAL_ERROR" by function disabling the ADC. */
}

__HAL_UNLOCK(hadc);

return tmp_hal_status;
}

 

 

 

0 REPLIES 0