2019-11-27 06:57 PM
I generated my code by stm32cubemx, and use ucpd1 as sink&dead battery, use ucpd2 as drp. But got USBPD_ERROR in USBPD_DPM_InitCore after execute " CHECK_PE_FUNCTION_CALL(USBPD_PE_Init(USBPD_PORT_0, (USBPD_SettingsTypeDef *)&DPM_Settings[USBPD_PORT_0], &DPM_Params[USBPD_PORT_0], &dpmCallbacks));
"
and USBPD_PE_Init success when just use ucpd1, why the added ucpd2 caused the ucpd1 USBPD_PE_Init error?
thanks.
Solved! Go to Solution.
2019-11-27 10:43 PM
This issue is linked to heap size used your project. You have to increase the 'Minimum heap size' in the "Project Manager[Project]" panel.
I advise you 0x800 instead of 0x400.
Useful debug function is the following one:
/* to get how much memory are dynamically allocated by the stack
the memory return is corresponding to 2 ports so if the application
managed only one port divide the value return by 2 */
stack_dynamemsize = USBPD_PE_GetMemoryConsumption();
(same problem as this thread)
2019-11-27 10:43 PM
This issue is linked to heap size used your project. You have to increase the 'Minimum heap size' in the "Project Manager[Project]" panel.
I advise you 0x800 instead of 0x400.
Useful debug function is the following one:
/* to get how much memory are dynamically allocated by the stack
the memory return is corresponding to 2 ports so if the application
managed only one port divide the value return by 2 */
stack_dynamemsize = USBPD_PE_GetMemoryConsumption();
(same problem as this thread)
2019-11-27 11:09 PM
thanks and it works.
2019-11-28 03:29 AM
Hello,
And I got another problem, when I set the breakpoint in USBPD_DPM_SNK_EvaluateCapabilities, and set USBPD_PORT_COUNT=1, and then I connect my pd power adapter with ucpd1 by typec line, it will trigger the breakpoint, and I can get the source capabilities from power adapter.
however, if I set USBPD_PORT_COUNT=2, after connect with ucpd1, this breakpoint will not trigger.
Defined symbols,
USE_FULL_LL_DRIVER
USBPD_PORT_COUNT=2
USBPDCORE_LIB_PD3_FULL
_RTOS
_DRP
USE_HAL_DRIVER
STM32G071xx
2019-11-29 06:25 AM
Hello,
I reproduced an issue with the following configuration:
Then CubeMX will generate a project with _DRP switch to cover both configurations.
We found an issue with this configuration. I suggest to apply the following patch in the file '.\Middlewares\ST\STM32_USBPD_Library\Devices\STM32G0XX\src\usbpd_cad_hw_if.c'
static uint32_t ManageStateAttached_SRC(uint8_t PortNum, USBPD_CAD_EVENT *pEvent, CCxPin_TypeDef *pCCXX)
{
(...)
/* evaluate CAD_tDebounce */
uint32_t CAD_tDebounce = HAL_GetTick() - _handle->CAD_tDebounce_start;
if (CAD_tDebounce > CAD_TSRCDISCONNECT_THRESHOLD)
{
HW_SignalDetachment(PortNum);
#ifdef _DRP
if (USBPD_TRUE == Ports[PortNum].settings->CAD_RoleToggle)
{
USBPDM1_AssertRd(PortNum);
}
#endif
Do not forget to add the handle for Port1 in 'UCPD1_2_IRQHandler' function:
/**
* @brief This function handles UCPD1 and UCPD2 interrupts / UCPD1 and UCPD2 wake-up interrupts through EXTI lines 32 and 33.
*/
void UCPD1_2_IRQHandler(void)
{
/* USER CODE BEGIN UCPD1_2_IRQn 0 */
extern void USBPD_PORT0_IRQHandler(void);
USBPD_PORT0_IRQHandler();
#if USBPD_PORT_COUNT == 2
extern void USBPD_PORT1_IRQHandler(void);
USBPD_PORT1_IRQHandler();
#endif
Sorry for the problem. We will fix it in the next G0 release.
2019-12-01 05:59 PM
It works for me, thank you very much.