cancel
Showing results for 
Search instead for 
Did you mean: 

STSPIN32G4 VDS故障

AijerJane0
Associate

您好。当我使用STSPIN32G4驱动三相桥控制BLDC时,MOE被自动置为0。通过读取STSPIN32G4内部的驱动状态寄存器,显示VDS位被置为1。我已经在SCREF上设置了足够高的参考电压(2V),但是这个故障仍然存在,导致我的驱动无法开始正常工作。硬件已经排查没有短路问题,运放采集的下桥臂电压也没有过流的迹象。我使用220uF 35V的陶瓷电容放置于直流母线,并连接了18V稳压管,母线电压12V,MOSFET用的AGM12N10AP。BLDC工作电压12V 额定电流1.8A。请问有什么解决方法?

 

0 REPLIES 0