cancel
Showing results for 
Search instead for 
Did you mean: 

Motor Bench Code & BLDC Winding Analysis

JayarajAnbalagan
Associate II

Hello All,

   Attached is the snapshot taken using logic analyser on PWM & Hall Effect TTL Signals. Trying with 446 & IHM08M1 – Open Loop.

D0 – PWM1 & D1 – PWM1 N

D2 – PWM2 & D3 – PWM2 N

D4 – PWM3 & D5 – PWM3 N

D6 – Hall Effect U

D7 – Hall Effect V

A0 – Hall Effect W (No extra digital channel, using the analog channel as digtal).

Practical Explanation Required at each cycle.

D6 rising edge makes PWM1 & PWM1N to operate until D3 rising edge –which winding is energised?

Like this, explanation required for 1 full cycle wrt to Phase Energising.

1 ACCEPTED SOLUTION

Accepted Solutions
2 REPLIES 2
JayarajAnbalagan
Associate II

Practical Explanation Required at each cycle.

D6 rising edge makes PWM1 & PWM1N to operate until D7 rising edge –which winding is energised?

Like this, explanation required for 1 full cycle wrt to Phase Energising.