2024-08-13 08:33 PM
Hello. I am using MCSDK 6.3.0, NUCLEO-F446RE, evalstdrive101. When the engine is running in Hall sensor mode. There are interruptions in operation due to signal failures from the Hall sensors. I tried two new engines of this type, the problem is repeated. Help solve this problem. Maybe it is possible to increase the value in the program code more than 0.1-10? Thank you!