2025-10-31 11:18 AM
Hello,
I'm using an EVSPIN32G4 with a Bodine BLDC motor (Hall-less). I used the motor profiler to get all the need motor settings and have compiled firmware. It spools up nicely but I can't get it to 6000RPM. The motor profiler says that the motor is capable of 6000 RPM. All of my settings appear to be correct.
I'm using a 48VDC supply capable of 12A. The motor cable says 6000 RPM, 7.8A, 48VDC.
This is a 2 pole pair motor. It seems that every change I make to try and resolve this tends to break something.
Does anyone have suggestions?
2025-11-03 6:36 AM
Hello @RinSxi,
"Flux-weakening control" or "overmodulation" features increase the maximum achievable speed.
You can also increase the PWM frequency while maintaining the maximum modulation index at 100%.
2025-11-10 7:23 AM
There isn’t enough information; you should verify whether the motor BEMF permits the motor to reach the desired speed given your bus voltage.