STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1731 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4879 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9575 Views
  • 5 replies
  • 3 kudos

AS5600 I2C Communication

Hi.I am trying to communicate with AS5600 Position Sensor. We are using I2C communication for this purpose. Using STM32F439ZIT6 chip , running chip at 168 MHZ clock. We are sommunicating with the sensor at Fast mode 400000 speed. Connection seems OK ...

V.D.T: by Associate
  • 3219 Views
  • 1 replies
  • 1 kudos

STM32 NUCLEO BOARD AND BOOSTXL-DRV8323RS

Hi,I am trying to run a 3-phase BLDC motor using the DRV8323 driver in 1xPWM mode with a Hall effect sensor. I am also using the Nucleo WB55RG board to generate a 20kHz PWM signal.The motor is spinning, but there is audible noise, which decreases onl...

Resolved! ACIM

Hi Is there any way to define a ACIM custom inverter?I have only 2 choices : FOC & 6-Stepwhat about ACIM custom board definition?Thanks.

Carador by Associate II
  • 1621 Views
  • 2 replies
  • 0 kudos

Resolved! Motor Control Board Customization

Hi every oneI have defined a custom motor and inverter successfully.Now I need to define custom features like a simple Digital output(LED for instance).Is there any way?or should I cut working on stmcubemx and continue coding after code generated by ...

Carador by Associate II
  • 3261 Views
  • 8 replies
  • 0 kudos