STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1730 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4875 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9575 Views
  • 5 replies
  • 3 kudos

Resolved! MCSDK 6.3.2 connectAlgo.log file not found

Hello,I got a error message during control project genaration"It is not possible to create a motor control project with the FOC algorithm using the selected hardware. No proper path for motor control signals was found for the following mandatory feat...

STSPIN32G4 can't work with external 3.3V

Dear Community,////  For new members joining the discussion, please refer to our second reply, where we’ve shared more details about the modifications and testing done on our board.Thank you in advance for your interest and support!I’m currently deve...

Sheng123_0-1743954957852.png
Sheng123 by Associate II
  • 1953 Views
  • 4 replies
  • 1 kudos

B-G431B-ESC1 firmware issues

Hi, I'm using a B-G431B-ESC1 to control a drone motor. My motor draw around 300W at maximum power. I have done a FOC firmware with Motor Workbench and it works very good with the load (propeller). I use sensor less speed feedback.But when I remove th...

jbigny by Associate
  • 864 Views
  • 1 replies
  • 0 kudos

Resolved! Why is there an STM32F103 on the B-G431B-ESC1 ?

Split from https://community.st.com/t5/stm32-mcus-motor-control/use-of-b-g431b-esc1-to-implement-my-own-algorithm/td-p/794170 as that is answered, and this is a new question.I needed to confirm this before making use of it.In the same thread, I have ...

davreg by Associate
  • 1606 Views
  • 3 replies
  • 5 kudos