STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1816 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4956 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9713 Views
  • 5 replies
  • 3 kudos

Resolved! How to create graphics using Motor Pilot

Hi all ,I’m currently using the EVSPIN32G development board to run six-step trapezoidal commutation.I’m using Motor Pilot version V1.2.12 with the MC_6STEP GUI.In the ST Motor Control tutorial under '6-step - Optimization and troubleshooting of senso...

未命名.png 未命名2.png
1123 by Associate II
  • 1091 Views
  • 1 replies
  • 0 kudos

STSPIN32G4 separate control and motor supplies

I developed a board for 3 ph motor control with a quadrature encoder that seems to work fine. Now my client would like to modify it to use separate supplies for control/logic and motor as is standard practice in the PLC/automation world.There are a c...

OscarM by Associate
  • 1732 Views
  • 2 replies
  • 1 kudos

Resolved! Emergency brake function for Position Control mode.

I am working on a project to drive a door using a PMSM motor in position control mode. I am trying to add an emergency brake function. In an emergency, when the operator pushes a button, motor should brake and then return to its starting position wit...

EDokm by Associate III
  • 1823 Views
  • 4 replies
  • 0 kudos

Weird noise on ADC - current sensing.

Hi, I'm developing a FOC board based on STM32G431RBT6 and I wanted to test the board in open loop before attempting to FOC.While testing for current sensing, I'm getting a lot of noise which messes up the measurement.I tried disconnecting the motor t...

karaoglu_0-1745360848307.png
karaoglu by Associate II
  • 3573 Views
  • 8 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.