STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1742 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4891 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9592 Views
  • 5 replies
  • 3 kudos

EVALSTDRIVE101 project file

Good day, I am wondering there is a way to access the project file for the EVALSTDRIVE101 demonstration board. I need to do a custom board based on it and only the Gerber files are available. I would appreciate any help. Thanks in advance  Mostafa   

Resolved! EVLSPIN32G0A1: Issue with compiling code

Hi,I got several FreeMarker template errors when I tried to compile the code to test out EVLSPIN32G0A1. It looks like all the files under MotorControl folder were affected by what I assume is the same error type (see attached picture).FreeMarker temp...

STMCubeIDE_Error.png
Bam by Associate II
  • 4437 Views
  • 8 replies
  • 0 kudos

Resolved! Error during generating project

Unable to generate motor control project using MCSDK 6.3.2The MCU is STM32G473CCU6"It is not possible to create a motor control project with the FOC algorithm using the selected hardware. No proper path for motor control signals was found for the fol...

Resolved! Unable to write to RAW Structur in MC Motor Pilot

Hello,I am trying to write to SPEED_RAMP using the Registers tab in MC Control Pilot, however I get the following error:ASPEP_RESP ERROR:ERROR_BAD_RAW_FORMATI am writing the data as follow for example: 6000;500Can someone help me find the right synth...

AnthonyK by Associate III
  • 756 Views
  • 1 replies
  • 0 kudos

Resolved! Motor Pilot (Observer + PLL) C1 / C2 Parameter Tuning

Hi all,I'm currently using Motor Pilot v1.2.12 and working with Observer + PLL mode for sensorless control. I see that there are parameters C1 and C2 available for tuning, but I'm not quite sure what each of them does and how they affect the motor co...

1123 by Associate II
  • 941 Views
  • 1 replies
  • 0 kudos

Cannot generate the IDE project

Hi, Community.When I try to generate an IDE project from the MotorControlWorkbench project I inherited, an error occurs.I checked both cases where a previous IDE project existed and where only the stwb6 file existed, but neither worked.The IDE, MX, a...

hijimasa by Associate II
  • 1863 Views
  • 4 replies
  • 0 kudos