STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1735 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4881 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9578 Views
  • 5 replies
  • 3 kudos

Project for B-G431B-ESC1

I need some working project for B-G431B-ESC1. I was trying to use MotorControl Workbench (X-CUBE-MCSDK). There is a project for the target but it creates an absolutely useless project. Some non-existing header files, no main file included in the proj...

Problem with Steval-Spin3202 Board

Hello everybody,I want to test a BLDC-Motor with the STEVAL-SPIN3202 board and the Motor Control workbench software. If I start the motor, I always get the message "start up failure" in the monitor of the Motor Control software and the motor doesn't ...

TKlei.5 by Associate III
  • 1209 Views
  • 2 replies
  • 0 kudos

Resolved! Motor Control Workbench and STM32CubeIDE doesn´t work !

Hi,i want to use Nucleo F303RE & IHM08M1 together to drive a PMSM. At first, I test the STM32CubeIDE with a led blink example, it works immediately.Then I test my motor, in the Motor Profiler, it works too. Now I want to use the MotorControl Workbenc...

0690X00000ArJweQAF.jpg 0690X00000ArJwjQAF.jpg 0690X00000ArJwoQAF.jpg 0690X00000ArJwtQAF.jpg

Motor control workbench generates... empty templates?

Hi,I installed the motor control software (5.4.1) on my computer and start my design for STM32G4. After code generation, I have numerous motor related file in the scr/ and inc/ directories but they are all empty (they only contain the classical ST he...

tarzan2 by Senior
  • 1536 Views
  • 3 replies
  • 0 kudos