STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1706 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4859 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9529 Views
  • 5 replies
  • 3 kudos

Resolved! STSPIN32G4 Error in generated code

Hello,I am using the STSPIN32G4 IOC file from MC Workbench for a motor control example. However, I encounter the following errors during the build process. Since these files are auto-generated, I can't directly fix them by declaring the missing eleme...

AsimAsrar_0-1719918843854.png
AsimAsrar by Associate II
  • 3891 Views
  • 8 replies
  • 0 kudos

Resolved! Adding user ADC on MCSDK 6.2.1

Dear all, currently, I'm making to control a BLDC motor from throttle using ADC1 channel 0. The MCU part number is STM32G0B1RBT6. I can read the ADC value successfully in SDK 5.4.8. The way how I do is I defined the ADC1-IN0 in Cube Mx and then I add...

Agga by Associate II
  • 2426 Views
  • 1 replies
  • 0 kudos

Controlling a servo Motor over BLE

Hi there, I'm trying to do a project that involves controlling a servo motor over the BLE I have a STM32wb15, i know my configuration is set up correct as I have copied a code from an example I have and the project works exactly as it should.My probl...

KaiP by Associate II
  • 3108 Views
  • 6 replies
  • 0 kudos

Resolved! 4x L6234PD with STM32F401

Hello ST expert,I'd like to control 4 300W motors with the BLDC L6234 and my STM32F401, but the problem is that I can't use 12 TIMERS and 12 GPIOs just for that, I need to interface other modules.Can I just use PWM/BLDC, and interface the two like th...

Paulo971 by Associate III
  • 2929 Views
  • 5 replies
  • 3 kudos

Resolved! Documentation of ASPEP Protocol?

As stated in UM1052, chapter 14 there is often a requirement to control a BLDC motor control board over a serial connection. The above manual describes the protocol used by older MCSDKs. But the latest MCSDK 5.Y.x seems to use a slightly different pr...

TThan by Associate III
  • 14616 Views
  • 12 replies
  • 8 kudos