cancel
Showing results for 
Search instead for 
Did you mean: 

Activations may exeed the size of all SRAM segments

ACapo
Associate II

I am trying to deploy a pre-trained Mobilenet model using STMCubeMX.ai, but I am facing some issue that I want to report.

Here the link of the project

https://github.com/alessandrocapotondi/mobilenet_stmcube_ai

Here the model I am using:

https://github.com/alessandrocapotondi/mobilenet_stmcube_ai/blob/master/keras_model/mobilenet_160_0_...

Here the resource usage of my model:

0690X0000089fpeQAA.png

600KB RAM for the activations and 1.79MB of weights. Unfortunally despite the "Green Light" given by the tool for the deployment on the STMH7432ZI on the device there is no segment that can fit such ammont of contigous data.

/* Specify the memory areas */
MEMORY
{
DTCMRAM (xrw)      : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D1 (xrw)      : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw)      : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw)      : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw)      : ORIGIN = 0x00000000, LENGTH = 64K
FLASH (rx)      : ORIGIN = 0x8000000, LENGTH = 2048K
}

Best,

Alessandro

1 ACCEPTED SOLUTION

Accepted Solutions
jean-michel.d
Senior

​Hello,

You have absolutly rights, unfortunaltly this check is currently not correctly supporting by the X-CUBE-AI tools.

br,

Jean-Michel

View solution in original post

4 REPLIES 4
jean-michel.d
Senior

​Hello,

You have absolutly rights, unfortunaltly this check is currently not correctly supporting by the X-CUBE-AI tools.

br,

Jean-Michel

Really thanks for your support!

Bassett.David
Associate III

As an aside - I like your test image!!!

😆