cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4xx CMSIS with clang compiler / many warnings

Posted on November 07, 2016 at 16:04

Hello,

I'm starting a project which uses an STM32F4xx as MCU. I want to use the STM32CubeMx tool for hardware setup and the ST CMSIS libraries for hardware control.

As compiler I want to use the Keil ARM v6.5 compiler (which is clang). Problem is, if I compile the CMSIS sources with the __GNUC__ definition, the build is successful but it generates really a lot of warnings (about 1000 for a few CMSIS files).

Now I'm wondering if there is a better way (or another library from ST?) to use the ST CMSIS files with clang or not?

Are there any experiences using the CMSIS with clang / arm compiler V6? (is this combination recommended?).

Thank you in advance!

#stm32f4 #compiler #cmsis
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
slimen
Senior
Posted on November 10, 2016 at 16:17

Hello,

What exactly did the warnings message say?

Maybe you should ensure that you are included the proper CMSIS library into your project and the paths are set up correctly.

Regards