2024-11-17 12:42 AM
Hi,
The X-Cube-Cryptolib is not in the list of STM32CubeMX software (I have the latest version).
and when I tried to add the downloaded zip file of the cryptolib expansion from the "From Local" in STM32CubeMX, it gives error.
1- It means that I can not add that lib directly into the STM32CubeMX ?
2- So I have to first make my project in STM32CubeMX and then add crypto library files manually in the project folder? (I use Keil software)
Thanks & Best Regards.
2024-11-17 5:15 AM
Hello @green_om_2006
The X-CUBE-CRYPTOLIB pack cannot be installed in CubeMX, however it can be included in the project generated by CubeMX.
For more details, please check this wiki: https://wiki.stmicroelectronics.cn/stm32mcu/wiki/Security:Getting_started_with_the_Cryptographic_Library
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-20 10:58 AM
Thanks for your reply, I followed the link step by step, but I get this error:
I checked all the compiler settings with a NUCLEO board project in the CryptoLib package too, They are all same with my own project....
I am using STM32L071.
Can you please help me fine and solve the problem?
Thanks & Best Regards.