cancel
Showing results for 
Search instead for 
Did you mean: 

HAL functions using archaic terms - why?

onderdelen
Associate III

Hi,

 

I am compiling the STM32U0 HAL library and I get errors like this one:

/Users/kiwanda/techniek/swexternals/STM32/HAL/Libraries/STM32U0xx_HAL_Driver/Inc/stm32u0xx_ll_comp.h: In function 'uint32_t LL_COMP_GetCommonWindowMode(const COMP_Common_TypeDef*)':
/Users/kiwanda/techniek/swexternals/STM32/HAL/Libraries/STM32U0xx_HAL_Driver/Inc/stm32u0xx_ll_comp.h:391:27: error: ISO C++17 does not allow 'register' storage class specifier [-Werror=register]
  391 |   register const uint32_t window_mode_comp_odd = (uint32_t)READ_BIT(COMPxy_COMMON->CSR_ODD, COMP_CSR_WINMODE);

I am using a C++ compiler and since C++14 the keyword register has been declared obsolete and useless. I fully agree with this step, all the more since we are writing SW here on ARM Cortex:

When writing software for ARM Cortex, which is a Load/Store architecture RISC processor, EVERYTHING goes through a register. The register keyword is therefore completely meaningless, useless and superfluous in this context.

I would like to ask ST to write the HAL libraries in such a way that they can also be used in modern contexts like the one I prefer to use. Checking the library with a C++ compiler is very effective since it finds anomalies and errors that (lax) C compiler disregard.

with best regards,

Ewout Boks

Ewout Boks

 

15 REPLIES 15
TDK
Super User

Mistakes happen. Looks like the "register" keyword is used exactly twice in the entire HAL library, just where you show it. Hardly a systemic issue.

If you feel a post has answered your question, please click "Accept as Solution".
gbm
Principal

register is not "completely meaningless". It may be used to ensure that error is signaled if & (address of) operator is used.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice

Well it depends on the compiler.

Ideally it can hold the values in the working registers, but auto variables can be held on the stack.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Super User

@onderdelen wrote:

I am using a C++ compiler


But the HAL is C - not C++

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

This is true.

But you should be able to write your app in C++ (which works generally).

When you #include the ST stuff a C++ compiler will complain about the register even if the #include is inside an extern "C" block.

Pavel A.
Super User

You can open an issue on GitHub against this code.

Saket_Om
ST Employee

Hello @onderdelen 

Thank you for bringing this issue to our attention.

I reported this internally.

Internal ticket number: 221904 (This is an internal tracking number and is not accessible or usable by customers).

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om

@mfgkw wrote:

When you #include the ST stuff a C++ compiler will complain...


right - didn't spot that it's in a header

 

PS:

@Saket_Om  This has come up before; eg, Is the "register" storage class specifier necessary in STM32 LL interfaces?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

C++ might complain or even forbid it, but I cannot find such information regarding plain C.
I suppose compilers will continue to support it to maintain backward compatibility.

On a related note, I learned C before the first ANSI standard, when there was only K&R.
And at that time, register and auto were still a thing.
As I heard the idea came from the original developers, using a PDP-11 system.
Where it probably made sense considering that the first toolchains had poor or no optimisation at all, due to memory constraints alone.