cancel
Showing results for 
Search instead for 
Did you mean: 

Can't obtain PHY timestamp data on incoming packets

marrr
Associate II

I am looking for a way to obtain the PHY timestamp of when Ethernet packets are received. I am using the board NUCLEO-F767ZI, which should support hardware timestamping. I can barely find documentation about this online, but some investigation led me to the function HAL_ETH_ReadData, which contains the following lines:

 

      /* Get timestamp high */
      heth->RxDescList.TimeStamp.TimeStampHigh = dmarxdesc->DESC7;
      /* Get timestamp low */
      heth->RxDescList.TimeStamp.TimeStampLow  = dmarxdesc->DESC6;

 

I can see that this code is executed. When I print the values of dmarxdesc->DESC7 and dmarxdesc->DESC6, I always get the value 0. I am wondering if this is some sort of configuration issue, or if I am missing something.

 

I'm not sure how important this is, but I'm using LwIP to handle my networking stack, which seems to work correctly on a higher-level (i.e. I can receive and send packets as expected).

 

Any hint as to what might be happening would be appreciated, thank you!

0 REPLIES 0