2020-02-10 06:51 PM
@Amel NASRI, @ranran, @Piranha, @Harrold, @Pavel A.
V2 of my fixes and improvements to H7_FW V1.5.0/V1.6.0 Ethernet...
Changes include
Find full details and source in the attached zip. V1 was posted to another developer's question. Please post any questions about V2 here.
Solved! Go to Solution.
2021-12-21 01:16 AM
Dear All,
Our Experts tried to answer almost all the limitations reported in this thread.
Please refer to this post for more details.
At this point, I suggest to close this discussion as it becomes difficult for us to follow it with the great number of comments.
Don't hesitate to submit your new posts asking new questions.
Thanks for all the ones involved to make ST solutions more efficient.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-02-11 04:56 PM
Errata to V2.0 documentation:
2020-02-14 09:37 PM
hi , can you please do share the user code also eg: #include "eth.h" and its sources.
2020-02-15 01:57 PM
How about putting it on Github so that it can be maintained?
2020-02-16 01:24 PM
> please do share the user code also eg: #include "eth.h" and its sources.
No I'll not share my phy code. This is like the BSP code of one of ST's example projects. You have to write this part yourself. Most likely it is limited value to you anyway. I've provided all the source files that ST's Cube would provide.
[edit] actually I've replaced MX_LWIP_Init and hadn't included that. FW_H7_V1.6.0 moves its call to MX_LWIP_Init to main, which is too early for my app, So in a USER CODE area above main() in main.c I've added “#define MX_LWIP_Init() /* Not used. */�? (without the quotes) and I've excluded LWIP\App\lwip.c from my builds and I've written my own. Other developers have posted Community already about mistakes in MX_LWIP_Init, e.g., incorrectly using netif_* where it should use netifapi_netif_*.
2020-02-16 01:41 PM
> How about putting it on Github so that it can be maintained?
I don't have a development board. So no common platform. Everyone's ethernetif.c would be different.
Finally, the ethernet bug-fixes task is finished where I work and I've other matters to attend.
2020-02-17 04:28 PM
To some questions from https://community.st.com/s/question/0D70X000007QuPr/cant-receive-ethernet-packets-in-stm32h750vb...
> tried to protect 32KB which covers all RX/TX buffers. It did not work.
Not sure. I'll describe the memories a bit. Hopefully something here helps.
Three memories areas need care:
Ideally the rx and tx buffers would be in D2. This is what I've done:
For the descriptors, this is what I've done: I'd not added memory barriers. MPU was easier. When ST fix their driver they ought add the necessary memory barriers and make it a Cube configuration so it defines macros that'd compile-in the memory barriers only if MPU's not used because they'd waste cycles if they're not needed.
This snippet from my map file shows the buffers and descriptors. The section names and miss-spellings were there before I arrived.
.EthTxBlock 0x30040000 0x4e30
0x30040000 . = ALIGN (0x4)
0x30040000 __ETH_TX_START = .
*(.TxArraySection)
.TxArraySection
0x30040000 0x4e30 Common\Eth\LWIP\Target\ethernetif.o
0x30040000 lwip_custom_ram_heap
0x30044e30 __ETH_TX_END = .
.EthDescriptorsBlock
0x30044e30 0x5d0
0x30045000 . = ALIGN (0x400)
*fill* 0x30044e30 0x1d0
0x30045000 __ETH_DESCRIPTORS_START = .
*(.RxDecripSection)
.RxDecripSection
0x30045000 0x180 Common\Eth\LWIP\Target\ethernetif.o
0x30045000 DMARxDscrTab
*(.TxDecripSection)
.TxDecripSection
0x30045180 0x180 Common\Eth\LWIP\Target\ethernetif.o
0x30045180 DMATxDscrTab
0x30045400 . = ALIGN (0x400)
*fill* 0x30045300 0x100
0x30045400 __ETH_DESCRIPTORS_END = .
.EthRxBlock 0x24000000 0x20000
0x24000000 . = ALIGN (0x20000)
0x24000000 __ETH_RX_START = .
*(.RxArraySection)
.RxArraySection
0x24000000 0x1fe00 Common\Eth\LWIP\Target\ethernetif.o
0x24000000 EthIfRxBuff
0x24020000 . = ALIGN (0x20000)
*fill* 0x2401fe00 0x200
0x24020000 __ETH_RX_END = .__ETH_TX_START is the start of the lwIP heap. In the source code I've provided, this is cached.
__ETH_DESCRIPTORS_START and section(".RxDecripSection") is the start of the descriptor memory. The section(".TxDecripSection") is a little higher in the memory. In the source code I've provided, this is an MPU region.
__ETH_RX_START and section(".RxArraySection") is the start of my rx buffers. In the source code I've provided, this is not-cached.
> you have used two regions starting from 0x30040000
Check my map-file snippet and details above. Check https://sourceware.org/binutils/docs/ld/SECTIONS.html#SECTIONS.
> where in stm32h7xx_hal_conf.h file I have to add those new defines
You don't. This stm32h7xx_hal_conf.h exists for (a) fixing defines like ETH_TX_DESC_CNT that the current Cube doesn't define properly, and (b) adding defines like ETH_PMT_IT_ENABLED which I've added to ST's ethernet driver source code as an example how they might improve that driver's implementation.
It's ethernetif.c job to integrate lwIP if you use it, your OS if you use one, the ethernet driver and your app.
For my changed ethernetif.c, you need to:
> I see that HArdFault_Handler() happens immediately
Perhaps D2 needs its clock enabled. See AN4891. In rev 3 it's on page 19. It's discussed elsewhere on Community.
> I could not find any definitions for this Callback function!.
My changed stm32h7xx_hal_eth.h file needs to be placed in an include directory your compiler searches before the "Drivers/STM32H7xx_HAL_Driver/Inc" directory.
> I am not going to use LWIP!
Assuming you're not meaning you're using a different stack, you'll need some way to queue packets where a packet may be a chains of buffers. Even bare-metal you'd implement queues. Even if you processed received packets immediately and discarded you'd still need queues... because your list of unused buffers is a queue. LwIP does it with struct pbuf. You'd need it for rx and tx. So your struct would need members for at least buffer length and next. For RxPoolInit, link all your buffers onto your free list. For RxBufferAlloc, allocate one buffer from your free list. For RxBuffFree, return one buffer to your free list. For RxPktAssemble, chain buffers by their next. For RxPktDiscard, return each buffer of a chain to your free list.
2020-02-17 11:32 PM
hi @alister ,
thank you.
unfortunately the solution doesnot works and breaks at below.
/* call user specified initialization function for netif */
if (init(netif) != ERR_OK) {
return NULL;
}
can somebody please share the references of MX_LWIP_Init issue?
may thanks in advance
2020-02-18 02:33 PM
> can somebody please share the references of MX_LWIP_Init issue?
MX_LWIP_Init hasn't changed between H7_FW V1.5.0 and H7_FW V1.6.0. It uses lwIP's raw API and you have to take care it's executed by only one thread at a time.
In H7_FW V1.5.0 it's called after FreeRTOS' scheduler starts, which could be unsafe.
In H7_FW V1.6.0 it's called before FreeRTOS' scheduler starts. So its using the lwIP raw API should be ok.
Reading MX_LWIP_Init, we see it sets the interface up or down based on whether the link is up or down. This looks like a bug. Piranha mentions it too at https://community.st.com/s/question/0D50X0000BOtfhnSQB/how-to-make-ethernet-and-lwip-working-on-stm32. It requires the init arg to netif_add, ethernetif_init in ethernetif.c to set the link status bit in the netif flags.
My opinion is you should flag the interface up as soon as you've initialised it, start with the link down, and flag the link up and down as you observe it change. This is in your phy code.
I've never used or debugged MX_LWIP_Init.
It's hardwired to use DHCP, whereas my app doesn't know whether to or not until later.
Perhaps it works. Not sure. Just it looks wrong.
> unfortunately the solution doesnot works and breaks at below.
The init arg to netif_add is ethernetif_init, and it's not returning ERR_OK or it's crashing.
Reading ethernetif_init, we see it can only return ERR_OK. So it's crashing somewhere in low_level_init.
You'll need to step the code to find why.
2020-03-06 04:44 AM
Hello, I would like to add ethernet support to my TouchGFX application.
I have got the lwIF directory from Cube and insert in TouchGFX Makefile with:
components := TouchGFX/gui target TouchGFX/generated/gui_generated LwIP
but I got many errors about include location, after many changes I have now this error if I use this define:
IP4_ADDR(&netmask, 255,255,255,255);:
Drivers/BSP/STM32746G-Discovery/stm32746g_discovery.c: In function 'udp_echo_init':
LwIP/include/lwip/ip4_addr.h:120:44: error: 'struct ip_addr' has no member named 'addr'; did you mean 'u_addr'?
#define IP4_ADDR(ipaddr, a,b,c,d) (ipaddr)->addr = PP_HTONL(LWIP_MAKEU32(a,b,c,d))