STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 USB Audio Class

Hello,I need to build a USB headset(mic+speaker) using STM32H742VIT6 for a project. I want the stm32h7 to be recognized as a audio device when connected to a PC/android device. Is this possible?This is my first time using a STM Board with cubeMX and ...

vo1d by Associate
  • 286 Views
  • 1 replies
  • 0 kudos

Resolved! STM32U575 - programming water marks..

Hi, I'm a bit stuck.   I'm trying to program watermarks for BANK2 (to make the entire bank secure so I can read the whole area using secure alias) for a custom boot-loader.   The code below is executing in secure context from BANK1 (and no bank swap)...

STM32F303C6T6 ADC DUAL REGULAR MODE

Hello, I am experiencing a problem with ADC1 and ADC2. I configured them in Dual Regular Simultaneous Mode, where ADC1 acts as the master and ADC2 acts as the slave. The ADC channel connections are as follows: ADC1 Channel 1: 24V_Sense ADC1 Channel...

Resolved! FMAC Cascade for SOS

Hi Together,I am currently trying to use the FMAC hardware accelerator. Normal usage already works. Now for numerical stability I want to implement the filter as second order sections (sos). According to RM0481:Cascaded filters must either be combine...

Resolved! Timer1 Interrupt is not generated

I am using Nucleo-F446RE board and trying to verify the TIM1 update interrupt and PWM, the PWM is generated but if i put a break point in the update interrupt it does not halt, what is the reason?int main(void) { /* USER CODE BEGIN 1 */ /* USER...

STuser2 by Senior III
  • 429 Views
  • 5 replies
  • 3 kudos