STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F415 SVD File

I can't find an svd file for the STM32F415 https://www.st.com/resource/en/svd/stm32f4_svd.zip does not contain a svd file for the STM32F415 series is one of the contained ones 100% compatible?  STM32F401.svd*  STM32F405.svd*  STM32F407.svd*  STM32F41...

ncore by Associate II
  • 5332 Views
  • 4 replies
  • 0 kudos

STM32F446 MP3 Player MCU Usage

Hi everyone, I'm developing an HMI with STM32F446. it has 800x480 display as well as a stack for communicating the devices with the CAN. Also, this stack must be updated in 4 milliseconds. Now also needing mp3 player and radio. For radio, a IC can be...

Resolved! How do I use HAL_SPI_Receive_DMA in conjunction with a receive buffer on the stack and caching enabled?

I am working with the STM32F760I-EVAL board and caching (SCB_EnableICache() and SCB_EnableDCache() are called) and MPU (MPU_Config() is called) are enabled. I am using DMA with SPI and if I transmit data, HAL_SPI_Transmit_DMA, I need to call SCB_Clea...

arnold_w by Senior II
  • 2535 Views
  • 4 replies
  • 0 kudos

STM32L475 Jumping to DFU

I am trying to figure out the details of how to jump to the internal bootloader on STM32L475. The following code works just fine on the STM32F405, but similar (updating the address obviously, which is actually the same) will not work on the L475.ldr ...