2020-07-16 12:54 AM
Hi there,
I am using STM32CubeIDE 1.3.0 with STM32L152x MCUs.
When using ST-Link GDB Server, STM32CubeIDE insists on updating Stlink firmware to the latest version (Now is V2.36.S7). After that I get the following errors:
ST-LINK SN : 49FF76068370565215201781
ST-LINK FW : V2J36S7
Voltage : 3.21V
SWD freq : 1800 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x429
Device name : STM32L100x6xxA/STM32L100x8xxA/STM32L100xBxxA/STM32L15xx6xxA/STM32L15xx8xxA/STM32L15xxBxxA
Flash size : 64 KBytes
Device type : MCU
Device CPU : Cortex-M3
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a07132.srec
File : ST-LINK_GDB_server_a07132.srec
Size : 9052 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Error: Flash loader cannot be loaded
Error: failed to erase memory
Encountered Error when opening E:\ST\STM32CubeIDE_1.3.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.3.0.202002181050\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
Using OpenOCD I encounter the following:
Open On-Chip Debugger 0.10.0+dev-01193-g5ce997d (2020-02-20-10:57)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
srst_only separate srst_nogate srst_open_drain connect_assert_srst
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
adapter speed: 8000 kHz
adapter_nsrst_delay: 100
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : clock speed 8000 kHz
Info : STLINK V2J36S7 (API v2) VID:PID 0483:3748
Info : using stlink api v2
Info : Target voltage: 3.179099
Info : SRST line asserted
Info : STM32L152RBTx.cpu: hardware has 6 breakpoints, 4 watchpoints
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Info : SRST line released
Error: timed out while waiting for target halted
TARGET: STM32L152RBTx.cpu - Not halted
Info : Device: STM32L1xx (Cat.2)
Info : STM32L flash size is 64kb, base address is 0x8000000
Info : SRST line asserted
Info : SRST line released
Error: timed out while waiting for target halted
TARGET: STM32L152RBTx.cpu - Not halted
Error: Target not halted
Error: failed erasing sectors 0 to 2
Error: flash_erase returned -304
shutdown command invoked
Info : dropped 'gdb' connection
But everything is OK with ST Link Utility Software. I think there is a problem with the latest STLink firmware version. Is there anyway to solve this problem or at least to prevent STM32CubeIDE from upgrading STLink firmware?
2020-07-16 2:09 PM
> at least to prevent STM32CubeIDE from upgrading STLink firmware?
+1
2020-07-31 8:52 AM
I think the problem is that I have not connected the Reset pin to the programmer. STM32CubeMXIDE can not handle this situation.
2020-07-31 10:33 AM
Seems CudeIDE doesn't use same drivers as STLink utility?
In IAR, the STLink properties has option to reset control or not by STLink, which typically is needed when the MCU goes deep low power clock stop modes.
2020-08-27 4:07 AM
CubeIde does have reset settings, for stlink gdb server or openocd, look in the debug configuration.
You can try without setting connect under reset mode and see if it works better.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.