cancel
Showing results for 
Search instead for 
Did you mean: 

Help Request: Ingrem Gaming Chair Board Wiring / Photos Needed

Matrim72
Visitor

 

Hello everyone,

I’m working on diagnosing and rewiring the control system for an Ingrem Veyron J20 gaming chair. The chair uses a servo module with an RJ45 connection to the handheld remote, and I’ve been tracing signals back to the main board (marked ST‑H801S‑V1.1 and ST‑H8‑CORE‑V2.1).

Here’s what I’ve established so far:

  • RJ45 pinout from the remote:

    • Pin 1 → Green (likely RX)

    • Pin 2 → Black (Ground)

    • Pin 3 → Yellow (TX??

    • Pin 4 → White (logic/handshake line, not VCC)

  • The board itself has a separate AC power feed.

  • With RJ45 disconnected, the board powers up fine (red LED lights). When RJ45 is wired incorrectly, the board fails to boot.

  • I believe the connections come from UART1 and COM20, but I don’t know how they should map to the RJ45 connector

:question_mark:What I Need

If anyone here owns an Ingrem Veyron J20 chair, could you please:

  • Photograph the main board (ST‑H801S / ST‑H8‑CORE) with the connectors attached.

  • Show the RJ45 wiring harness and how the colored wires (green, black, yellow, white, red) are mapped.

  • Confirm whether the white line is actually used for handshake or left floating.


Why This Matters

I’m trying to restore full functionality (servo + remote control). Having a clear photo of the board with connections would save a lot of guesswork and confirm the correct pinout.

Any help, teardown shots, or wiring notes from fellow Ingrem chair owners would be hugely appreciated.

Thanks in advance

IMG_2299.jpeg

0 REPLIES 0