2024-05-25 01:40 PM
Hi,
I have a X-NUCLEO-NFC08A1 and trying to use ST25R3916B RFAL library with nRF5340 from nordic semiconductor. SPI communication and initialization are working. I am running demoCycle() function from demo_polling.c. However, in the logs, I receive always null as ID or Block Data.
Toggling Wake Up mode OFF
D: ISO14443A/NFC-A card found. UID: (null)
D: Read Block: OK Data: (null)
D: Toggling Wake Up mode ON
When I put my phone close to reader I receive following:
NFCA Passive ISO-DEP device found. UID: (null)
D: Select NDEF Application: OK Data: (null)
D: Select CC: OK Data: (null)
D: Read CC: OK Data: (null)
D: Toggling Wake Up mode OFF
Why is it not reading any data? How can I run the demo?
Solved! Go to Solution.
2024-05-25 02:11 PM
Hi,
it is likely that USE_LOGGER is not defined in your port and therefore hex2Str returns NULL.
Make sure to add USE_LOGGER in your compiler global defines. There should be as well ST25R3916B as global define.
Rgds
BT
2024-05-25 02:11 PM
Hi,
it is likely that USE_LOGGER is not defined in your port and therefore hex2Str returns NULL.
Make sure to add USE_LOGGER in your compiler global defines. There should be as well ST25R3916B as global define.
Rgds
BT
2024-05-25 02:53 PM - edited 2024-05-25 02:55 PM
Jackpot! Thank you, now it is printing hex strings.