2025-08-04 7:24 AM
Hi all,
I am using ST25R200 and NTAG215 from NXP. I configured RFAL to use T2T and NFCA
#define RFAL_FEATURE_LISTEN_MODE false /*!< Enable/Disable RFAL support for Listen Mode */
#define RFAL_FEATURE_WAKEUP_MODE true /*!< Enable/Disable RFAL support for the Wake-Up mode */
#define RFAL_FEATURE_LOWPOWER_MODE true /*!< Enable/Disable RFAL support for the Low Power mode */
#define RFAL_FEATURE_NFCA true /*!< Enable/Disable RFAL support for NFC-A (ISO14443A) */
#define RFAL_FEATURE_NFCB false /*!< Enable/Disable RFAL support for NFC-B (ISO14443B) */
#define RFAL_FEATURE_NFCF false /*!< Enable/Disable RFAL support for NFC-F (FeliCa) */
#define RFAL_FEATURE_NFCV false /*!< Enable/Disable RFAL support for NFC-V (ISO15693) */
#define RFAL_FEATURE_T1T false /*!< Enable/Disable RFAL support for T1T (Topaz) */
#define RFAL_FEATURE_T2T true /*!< Enable/Disable RFAL support for T2T */
#define RFAL_FEATURE_T4T false /*!< Enable/Disable RFAL support for T4T */
#define RFAL_FEATURE_ST25TB false /*!< Enable/Disable RFAL support for ST25TB */
#define RFAL_FEATURE_ST25xV false /*!< Enable/Disable RFAL support for ST25TV/ST25DV */
#define RFAL_FEATURE_DYNAMIC_ANALOG_CONFIG false /*!< Enable/Disable Analog Configs to be dynamically updated (RAM) */
#define RFAL_FEATURE_DPO false /*!< Enable/Disable RFAL Dynamic Power Output support */
#define RFAL_FEATURE_ISO_DEP true /*!< Enable/Disable RFAL support for ISO-DEP (ISO14443-4) */
#define RFAL_FEATURE_ISO_DEP_POLL true /*!< Enable/Disable RFAL support for Poller mode (PCD) ISO-DEP (ISO14443-4) */
#define RFAL_FEATURE_ISO_DEP_LISTEN false /*!< Enable/Disable RFAL support for Listen mode (PICC) ISO-DEP (ISO14443-4) */
#define RFAL_FEATURE_NFC_DEP false /*!< Enable/Disable RFAL support for NFC-DEP (NFCIP1/P2P) */
So far detecting the Tag and reading and writing works just fine by using:
rfalT2TPollerWrite
rfalT2TPollerReadHowever, I am not sure how I can use the password protection feature from the nfc tag. I would like to be able to set a password and then to read and write from memory using the set password. What API Methods would I use for that? I am quite confused with all the different types and Feature configurations. I only want to use and support T2T tags, which should be able to handle password protection.
Solved! Go to Solution.
2025-08-04 8:21 AM
Hi,
The rfal_t2t.c file implements NFC Type 2 Tag (T2T) commands as specified by the NFC Forum:
Password protection is a proprietary feature not defined by the NFC standard. It relies on a proprietary PWD_AUTH command (1Bh) described in the tag datasheet. To implement support for the PWD_AUTH command, duplicate the rfalT2TPollerWrite function as rfalT2TPollerPwdAuth and modify it to send the 1Bh command with the 4-byte password and to check the returned PACK value.
The rfalT2TPollerWrite function can be used to write various configuration pages to update AUTH0, PWD, and PACK values. For more details on the authentication, contact the manufacturer of this tag.
Rgds
BT
2025-08-04 8:21 AM
Hi,
The rfal_t2t.c file implements NFC Type 2 Tag (T2T) commands as specified by the NFC Forum:
Password protection is a proprietary feature not defined by the NFC standard. It relies on a proprietary PWD_AUTH command (1Bh) described in the tag datasheet. To implement support for the PWD_AUTH command, duplicate the rfalT2TPollerWrite function as rfalT2TPollerPwdAuth and modify it to send the 1Bh command with the 4-byte password and to check the returned PACK value.
The rfalT2TPollerWrite function can be used to write various configuration pages to update AUTH0, PWD, and PACK values. For more details on the authentication, contact the manufacturer of this tag.
Rgds
BT