2025-10-07 2:15 AM - last edited on 2025-10-08 4:21 AM by mƎALLEm
Updated the title to be inline with ST community rules.
Hi all! So I am looking for a standard antenna which would be suitable for ST25R100-CMET (IC Reader 13.56MHZ 24 UFQFN). This will be used in an alarm module with a lock, so please suggest! Thank you!
Solved! Go to Solution.
2025-10-07 2:26 AM
2025-10-07 2:26 AM
2025-10-08 4:18 AM
Hello Vibrao,
there are different type of NFC antennas.
Typically the NFC antenna is defined by the available space and is chosen to meet the performance criteria.
The good news is, that our ST25R100/200/300 devices can be used with all of them.
I would recommend you the following application notes for further details about the antenna matching:
Please let us know, if you have further questions!
br Travis