2023-09-28 4:53 AM
I am using the ST25R3918 and the 'pollingTagDetect' example from the RFAL library. This chip does not have the ST25R3916_CMD_TEST_ACCESS register.
How can I modify this library?
Solved! Go to Solution.
2023-11-06 3:07 AM - edited 2023-11-06 3:11 AM
Hi,
I explain how I figured it out.
Firstly, I purchased the STM32L476 Nucleo-64 and adjusted my system clock values to match the example NFC06A1_PollingTagDetect's system clock.
I changed the variable value from uint8_t globalCommProtectCnt; to uint8_t globalCommProtectCnt = 0;.
Next, I adjusted the resistor of my PCB antenna matching component.
It is working now and I'm using STM32F0 I can use other STM boards.
Best regards,
ZD
2023-11-06 4:23 AM
Hi,
thanks for your feedback.
The C language guaranties that uninitialized global variable are implicitly initialized to 0 (practically such variables are allocated in the .bss segment which is memset to 0 by the c runtime initialization). Therefore changing uint8_t globalCommProtectCnt; to uint8_t globalCommProtectCnt = 0;. has no real effect.
I believe that the real fix is " I adjusted the resistor of my PCB antenna matching component."
Rgds
BT
2023-11-08 2:30 AM
Hi,
I believe too, now everything is okay.
Rgds
ZD