ST25 NFC/RFID tags and readers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I am using ST25R3911DISCOComm.dll and the lib in a QT application. Using MSVC 2019 32-bit configuration I am able to get my application running using the 'Debug' sub-configuration only. If I use the 'Release' the application crashes immediately.

I am using ST25R3911DISCOComm.dll and the lib in a QT application. Using MSVC 2019 32-bit configuration I am able to get my application running using the 'Debug' sub-configuration only. If I use the 'Release' the application crashes immediately. My s...

TOzya.1 by Associate II
  • 329 Views
  • 5 replies
  • 0 kudos

Resolved! Questions about ST25DV16 + Nordic 52832

Hello,I'm using adafruit ST25DV module with Nordic 52832 as host MCU, and porting the code to host bases on the ST25DV_DISCOVERY_FW_V1.1.2 demo, then encountered below issues:1) In the demo, after enabling FTM, host MCU will keep monitoring the it st...

KLam.11 by Associate II
  • 640 Views
  • 15 replies
  • 0 kudos

Resolved! energy efficiency on NFC06A1 board

Hi, As I want to measure the energy efficiency on the NFC06A1 board. Could you provide the testing position of the VDD_RF pin on PCB board? And do you have a clear tutorial about your antenna auto-tuning system? The third problem is about AAT technol...

0693W00000Dn47QQAR.png 0693W00000Dn47LQAR.png 0693W00000Dn47GQAR.png 0693W00000Dn47BQAR.png
TZhou.2 by Associate II
  • 331 Views
  • 3 replies
  • 0 kudos

Resolved! NFC Library

When I download The ST25 embedded NFC library (STSW-ST25R-LIB) , I get an zip file.Only one file inside, "ST25NFCEmbeddedLibSrc_ST25R95_1.3.0.exe".I got an execute file ? The Software Type is "Source code"? STM32CubeIDE support MAC OS, but library do...

Lwang1 by Associate II
  • 295 Views
  • 3 replies
  • 0 kudos