ST25 NFC/RFID tags and readers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST25R3916 FTM RF Message Read Failed

Hello,I am using ST25R3916 based X-Nucleo-NFC06A1 with Raspberry-Pi to read data from ST24DC64KC tag (which is custom board) using FTM. I am able to read the message using  rfalST25xVPollerReadMessage(), But only if length is below 128. If I am tryin...

ADant.1 by Associate II
  • 1239 Views
  • 4 replies
  • 0 kudos

Resolved! ST25R3911 high cpu use

I have integrated the ST25R3911B into an ARM64 Linux development board, using rfal_v1.3 for communication via SPI.I am able to poll and read cards successfully, but I've observed higher CPU usage.Upon inspecting the perf.svg, it appears that the st25...

zhaocz by Associate II
  • 3315 Views
  • 24 replies
  • 0 kudos

Resolved! stream mode configuration of the ST25R3911B

    我目前在使用的芯片是ST25R3911B,准备用于和我的另一个设备进行自定义协议的通信,但我在规格书内找不到关于“stream mode”的配置流程,想知道在什么地方可以找到流模式的参考例程。    另外看到透明模式似乎也可以实现自定义协议的通信,但是规格书内提供的配置信息太少,能否提供透明模式的配置流程。The following uses machine translation:    I am currently using the chip ST25R3911B for cust...

Jack_Chen by Associate III
  • 896 Views
  • 2 replies
  • 0 kudos

Resolved! How about STEVAL-SMARTAG1 No power mode?

Currently purchased with the STEVAL-SMARTAG1, it was discovered that the capability collected through the ST25 powers the L0 via EH pin VDD while collecting data from the sensor. I need to collect signals by thermocouple, which is the same transmissi...

Resolved! IOS NFC-TAP doesn't read FTM buffer

Hi everyone, I would like use FTM feature of ST25DV.I develop the code to write EEPROM and buffer of FTM, I can read this buffer with developed Kit and ST25PC-NFC software.But I can't use APP for IOS NFC-TAP because it doesn't read FTM buffer. why?

AGarc.8 by Associate
  • 731 Views
  • 3 replies
  • 0 kudos