ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CR95HF Write command

Posted on November 24, 2013 at 18:19I use the CR95HF chip for reading and writing data in the NFC forumtag Type 2 Tag (NTAG203F). I can read the data, but can not write data to Tag, although NTAG203F is writable. When I send a command to write data,...

Resolved! STSW-95HF003 Document

Posted on November 05, 2013 at 16:29Hello, I want to download the http://www.st.com/web/en/catalog/tools/FM147/SC1871/PF259363♯, the Excel sheet named STSW-95HF003. Can you fix the link, because it is broken, it gives a 404 Error. Or you can give a ...

tacsik by Associate II
  • 1352 Views
  • 3 replies
  • 0 kudos

Resolved! Enabling M24LR16E-R Energy Harvester

Posted on October 18, 2013 at 11:58Hi to all,I'm using a self-made eval board based on the M24LR16E-R dual EEPROM chip. It is very simple as it consists of the EEPROM chip, filter capacitors, pull-up resistors and, obviously the antenna.RF signal is...

danilo by Associate
  • 1001 Views
  • 1 replies
  • 0 kudos

Resolved! M24LR-discovery RF range versus external 3V3

Posted on August 14, 2013 at 22:24Hello all, I have been trying the M24LR-discovery board.  Without applying an external 3V3 supply to the board, the operational range appears to be only about 1.5cm (less than one inch).  There is an antenna design ...

mneary by Associate
  • 1196 Views
  • 3 replies
  • 0 kudos

Resolved! CR95HF error code 4

Posted on September 25, 2013 at 16:57occasionally when I send a  CR95HFDll_SendReceive command, I get error code 4 back. 5 I understand - the USB is not connected, so I simply reconnect, but 4 is a communication error. How can I recover from this in...

duncan by Associate II
  • 1062 Views
  • 2 replies
  • 0 kudos

Resolved! Issues with Programming CR95HF/M24LR in VB.net

Posted on September 04, 2013 at 11:55Hi there, I am using a CR95HF board from a M24LR discovery kit to read data from a device. If I use the dual-interface EEPROM software from the ST website, select Reader Application and select M24LR64A, then clic...

duncan by Associate II
  • 2097 Views
  • 6 replies
  • 0 kudos