ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CR95HF: Tag removal detection

Posted on May 06, 2014 at 11:42Detecting the presence of tags with the CR95HF works fine. But is it possible to detect the removal of a tag within the antenna field? I was thinking about polling the Tag Detect command with a very short timeout. As l...

g23 by Associate
  • 747 Views
  • 1 replies
  • 0 kudos

Resolved! M24LR16E - I2C communication

Posted on May 14, 2014 at 15:03Hello,I wish to use the M24LR16E as a NFC tag. In order to do this I have an ANT1-M24LR16E, a CR95HF and an Aardvark for the I2C communication.With the M24LRxx_Application_Software I send a text through the RF (with th...

adina by Associate
  • 753 Views
  • 1 replies
  • 0 kudos

Resolved! Solved: is password required for RF-OFF via I2C?

Posted on April 23, 2014 at 11:19Hi, can I disable the RF field of the M24SR by writing a 0x00 in the 0x06 offset of the system file 0xE101? Do I need to send any password-related command before? Can anybody please the NAK question in [DEAD LINK /pu...

joaquim by Associate III
  • 667 Views
  • 1 replies
  • 0 kudos

Resolved! Solved: Another mistake in M24SR datasheet

Posted on April 02, 2014 at 12:27Hi, as [DEAD LINK /public/STe2ecommunities/memories/Lists/M24SR%20Series/Flat.aspx?RootFolder=/public/STe2ecommunities/memories/Lists/M24SR%20Series/M24SR%20-%20mistake%20in%20table%2067%20Datasheet&FolderCTID=0x0120...

joaquim by Associate III
  • 1060 Views
  • 3 replies
  • 0 kudos

Resolved! Demo CR95HF-A ISO 15963 max range

Posted on January 23, 2014 at 11:23Hi, I'm trying to achieve the maximum reading range from my demoboard CR95HF-A with a ISO 15693 tag (LRi2K). Until now I've obtained best results with modulation-index 10% and gain 34dB by writing 0x50 to ARC_B reg...

pieretti by Associate II
  • 2537 Views
  • 13 replies
  • 0 kudos

Resolved! M24LR04E-R time to ready from power-up?

Posted on March 17, 2014 at 12:24Hi all, I'm looking for an indication of worst-case time-to-ready: i.e. from power-up - assume external VCC, not induced power - to fully commandable from I2C. I've searched the datasheet (DocID022208 rev 8) from end...

Jon Green by Associate II
  • 1129 Views
  • 3 replies
  • 0 kudos

Resolved! Solved: M24SR not working when soldering headers :(

Posted on March 20, 2014 at 10:58Hi everybody!It's my first post here and it's my first time working with STMicroElectronics stuff so please be aware I will probably ask very simple or even stupid questions. Please have some patience with me! :)By t...

0690X00000603NmQAI.jpg
joaquim by Associate III
  • 1028 Views
  • 4 replies
  • 0 kudos

Resolved! Bug in CR95HF development software

Posted on March 19, 2014 at 13:44First of all: I really like the software for DEMO-CR95HF-A. But there is an issue with the scripting tool: The command CR95HF_ISO14443-A_SEND_APDU, 00A4040007a0000000030000 should be translated intoCR95HFDLL_SENDRECV...