Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L6470H disc board communication problem

Posted on July 24, 2015 at 04:18hii got a L6470H disc board and try to run the source code from (dSPIN_Firmware_Library_STM32) and (dSPIN Discovery Kit) project both of them get SPI communication fail: any read of spi get 0xFF, the board is new and ...

tech problem with L6470H disc board

Posted on July 23, 2015 at 09:59Hi, i get start to test a L6470H discovery board and got some problems:1.i try to connect board and pc with usb cable but it shows unknow device in windows device manager in win7-64bit but works fine in win xp 32bit.(...

L6470H disc board problem

Posted on September 06, 2015 at 05:49hi, i bought a 6470h disc board and found a problem that spi communication always fail, whatever spi command send from mcu the driver always back 0xff. and i checked spi signal with oscilloscope, the only thing i...

Implement Emergency Stop on L6470

Posted on September 01, 2015 at 22:16HI, I am using an L6470 and have a situation where I must stop motion immediately if an obstruction (think someone's hand) crosses an IR beam. Motion must stop immediately and not via any commands since there can...

spelger by Associate II
  • 578 Views
  • 0 replies
  • 0 kudos

L6482H OVER CURRENT

Posted on July 21, 2015 at 20:55I need some help on a drive controller that I designed that uses two L6482's. The problemis sometimes while running, one motor will shut off. Reading the status register shows an over current condition. The testing cu...

rengholm by Associate II
  • 4663 Views
  • 5 replies
  • 0 kudos

Need assistance with SPWM Motor Control for ACIM

Posted on August 12, 2015 at 10:02HiI have made a post about my problem here: https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32F103%20PWM%20Interrupt%20not%20workingIf anyone is able to assist me it would be much appreciated....

High Voltage AC limiting circuit

Posted on May 11, 2015 at 10:01Apllication note AN2625: Theproblem which i am facing is that there are very large voltage spike at Vds which are not shown in the application note .And what aret he design creteria for selecting R2 and R4. Regards, Pa...

L6470 /Soyo SY57ST56-1206A lacks torque at high speed

Posted on August 01, 2015 at 02:59Hello all, I have a L6470 based board powering a 1.2A/ 12V Soyo SY57ST56-1206A motor, and at low speeds it has the expected torque, but it falls off drastically above 300 pps, and by 600 pps it doesn't move at all u...

rx7man by Associate
  • 561 Views
  • 1 replies
  • 0 kudos