Skip to main content
Associate III
Nov 12, 2025 9:51 AM UTC
Solved

STM32U575 - available pins for SPI / QSPI

@Issamos  

Am planning to Quad SPI, which port we can use, i cannot able to find the data sheet below listed pins can use 
Controller -STM32U575VIT6 (LQFP64, 10 × 10 mm)

  • QSPI_CLK → PB2
  • QSPI_NCS → PB6
  • QSPI_IO0 → PD11
  • QSPI_IO1 → PD12
  • QSPI_IO2 → PE2
  • QSPI_IO3 → PE3


  • Pls suggest the pins details 



Issamos
IssamosBest answer
Super User
Nov 12, 2025 10:54 AM UTC

Hello @HA2375- 

here is a choice for two SPI interfaces and an octospi set for QUADSPI. you can use the pins on the screenshot:

Issamos_0-1762944888113.png

Best Regards.

II

8 replies

Issamos
Super User
Nov 12, 2025 10:04 AM UTC

Hello @HA2375- 

The easiest way to do that is to create a project using the STM32CubeMX V6.15.0 and selecting the STM32U575VIT6 as MCU for this project. After that, enable one of the available octo-spi interfaces (the one that you want to use) and set the mode to quad-spi. The GPIOd that you need will be set for this interface on the Graphic. You can use those Pins.

Ps: please don’t forget to select a best answer for your previous question.

Best Regards.

II

HA2375-Author
Associate III
Nov 12, 2025 10:08 AM UTC

@Issamos  yeah sure definitely.

Can You Confirm the Pins and Ports for the QUAD SPI STM32U575VIT6 (LQFP64, 10 × 10 mm) 

Am bit confused and am not get much documents about this 

 thanks.

HA2375-Author
Associate III
Nov 12, 2025 10:20 AM UTC

 @Issamos 

 Below mentioned Controller part we are Going to use
 STM32U575RIT6
 Pls Suggest or confirm the Quad SPI and Octa spi ports list and 2 SPI Ports list. 
waiting for your Replay 
thanks.

 

Issamos
Super User
Nov 12, 2025 10:19 AM UTC

Hello @HA2375- 

Those are not the correct pins. Please try the method I’ve mentioned before. It should be the easiest way.

Best Regards.

II