cancel
Showing results for 
Search instead for 
Did you mean: 

LPUART not working in STM32L053R8T6

JishnuE
Associate

Hi,

I tried to connect a LoRa module to an STM32 controller using LPUART1. I am using HSI as the clock source and have configured PB10 and PB11 as UART RX and TX, respectively. However, I am not receiving any data while using the HAL driver API. In the Arduino IDE, I used the dedicated library for my LoRa module, and it worked.

Could anyone please explain why I am facing this issue and why I cannot replicate the same functionality in STM32CubeIDE?

 

Note Baud rate is 9600

Thanks.

1 REPLY 1
TDK
Super User

If it's "not working," there's probably a bug in your code somewhere. Nobody has clairvoyance here. You'll need to show enough of what you're doing in order to spot the error. 

If you feel a post has answered your question, please click "Accept as Solution".