cancel
Showing results for 
Search instead for 
Did you mean: 

Drive Nema 17/23 stepper motor

Lukas201
Associate

Hello everyone,

as part of a project, I would like to control a NEMA 17 or 23 stepper motor via UART. A TMC2209 driver is being used, and the software environment is STM32 CubeIDE. For reasons we cannot explain, we are unable to get the motor running.

I am open to any tips that could help us get the motor working. The code can also be provided if needed.

Thanks in advance for all feedback :)

1 REPLY 1
mƎALLEm
ST Employee

Hello Lucas and welcome to the ST community,

Read also a related thread here.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.