Others: STM32 MCUs related

Find out more about STM32 implementations with external components, discuss use cases, and discover how to use new tools and ST components.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RAK3172 Module boot mode issues

Hello,I hope you are doing well.I am currently facing critical issues with my RAK3172 module and STM32Cube Programmer setup and urgently need your technical support. Here are the details:1. RAK3172 Module Issue (LoRa P2P Communication)Initially, the ...

hetal by Associate
  • 820 Views
  • 1 replies
  • 0 kudos

Resolved! OTA firmware update using W5500

Hii, I want to update the firmware of my STM32H723ZGT6 microcontroller. Here, I want to send firmware file from server to W5500 Wiznet IC then I want that this firmware should load in to the microcontroller flash and it should update the program so c...

Aries16 by Associate II
  • 1080 Views
  • 2 replies
  • 1 kudos

Micrium task creation failure on STM32L4R9

Hi, I am using STM32l4R9 and using uCosIII Os with 16MHz CPU frequency. The project works fine with bare metal but getting failed when creating micrium tasks. The same micrium project works fine with 48MHz CPU frequency. TIA!  

P..1 by Associate
  • 709 Views
  • 1 replies
  • 0 kudos

Problem with Single Step STM32F7

Posted on December 07, 2016 at 21:47 There is a problem with IDE debuggers for STM32F7, and as I understand, all ARM M7 core based processors. With other CORTEX controllers, when a debbuger pauses or hits a breakpoint, the debugger stops interrupt p...