Others: STM32 MCUs related

Find out more about STM32 implementations with external components, discuss use cases, and discover how to use new tools and ST components.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 Keil V5 & RTX & Custom Bootloader

Posted on August 18, 2014 at 12:37Hi all,After some battle i was able to set a jump from my custom Bootloader to the App using in Keil V5.Custom Bootloader resides in IROM 0x08000000App resides in IROM 0x08020000Need to set both mem addr in the Ke...

afduarte by Associate II
  • 1822 Views
  • 3 replies
  • 0 kudos

two weired error in a c programin keil

Posted on September 24, 2014 at 18:34hi every bodyi declared a void function[CODE]void SPI_MFRC522_Init(void){..............}[/CODE]& used it in a main program[CODE]void RC522_IO_Init(void){ GPIO_InitTypeDef GPIO_InitStruct; RCC_APB2PeriphClockCmd(R...

0690X00000602xoQAA.jpg
mhdizgah by Associate II
  • 888 Views
  • 3 replies
  • 0 kudos

crating new stm32f103 project in keil

Posted on August 31, 2014 at 06:52hi every bodyi have some question about creating a new project becouse of my serious problems with it:in version 4 we copy header files of mcu &cmsis library to the projects folder,& i saw some learning cources do t...

mhdizgah by Associate II
  • 1908 Views
  • 6 replies
  • 0 kudos

Stm32CubeMX + CoIDE

Posted on August 15, 2014 at 00:23Hello everybody! I use CoIDE for develop applications to stm32f4 series. I checked Stm32CubeMx. This is a very good tool but not able to generate to CoIDE. I write a project converter tool, that can be convert TrueS...

totti001 by Associate II
  • 753 Views
  • 2 replies
  • 0 kudos

STM32CubeMX V4.3 & Keil MDK 4.7 linking problem

Posted on July 20, 2014 at 15:56Hi, When I make Project, generate code, open Project in MDK, Close NKD, Change Project, generate again, open MDK,....... several times then following happens: 1.) every 2,3,4th times, when I build all of MDK Project, ...

Osto by Senior
  • 1290 Views
  • 4 replies
  • 0 kudos

External RAM for stm32 eval2 board

Posted on July 30, 2014 at 14:14I am working on a project on the stm32 eval2 board that requires about 600 kB of RAM.  Do I need to add external memory to the FMC bus? Or is all the memory I need already provided with the board.  I do not understand...