Others: STM32 MCUs related

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PIL mode with STM32 Embedded Target, IAR, and J-LINK

Posted on January 13, 2014 at 13:31HiI've recently been playing the with STM32 Discovery using IAR and J-LINK and Simulink.  I've managed to set everything up okay, and can deploy some of the test Simulink models that ship with the STM32 Embedded Ta...

daryl by Associate II
  • 2605 Views
  • 13 replies
  • 0 kudos

stm32l100rb eeprom size 2kb or 4kb?

Posted on January 17, 2014 at 14:55In the http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00078075.pdf of the micro it's listed that the EEPROM size is of 2Kb.In the http://www.st.com/st-web-ui/static/active/en/r...

dfacchin by Associate II
  • 733 Views
  • 3 replies
  • 0 kudos

Debugger stuck at Hardware fault

Posted on January 08, 2014 at 03:33We just bought ST-Link to debug our software. Everything works great with Atollic and Seger J-Link with ST32F407 chip.But when we switch to ST-Link, we can flash the chip, but when start the debugger (in JTAG mode)...

0690X00000602qNQAQ.jpg 0690X00000602qSQAQ.jpg 0690X00000602qXQAQ.jpg 0690X00000602qYQAQ.jpg
mayank by Associate II
  • 1460 Views
  • 8 replies
  • 0 kudos

STM32F4 - Keil UDP example?

Posted on January 02, 2014 at 19:49Does anyone know where I can get a hold of an example using an stm32f407, UDP, and Keil TCPnet library?I am using:STM32F407VGT6Micrel KSZ8721BLKeil UV4RTXTCPnetI have been trying to get a UDP broadcaster to work to...

dibs by Associate II
  • 525 Views
  • 1 replies
  • 0 kudos

I2C Ack error

Posted on December 27, 2013 at 08:26dear all       i am using an I2C protocol to interface micro-controller with EEPROM, i am facing an Ack error , i kindly request you all to help me regarding this error , i have attached the file plz have a look i...

HSE can not be ready at debug

Posted on July 09, 2013 at 09:34 In mySetSysClockTo72 function, there is /* Wait till HSE is ready and if Time out is reached exit */ do { HSEStatus = RCC->CR & RCC_CR_HSERDY; StartUpCounter++; } while((HSEStatus == 0) && (Star...

auzgec by Associate II
  • 2773 Views
  • 9 replies
  • 0 kudos

.lib file in IAR Embedded workbench

Posted on July 05, 2012 at 04:57I need to program some algorithms to STM32F103. I want to create a .lib file similar to the attached files, then i want to link in IAR embedded workbench project & call the algorithms.The attached files are from a fir...

harinath by Associate III
  • 2891 Views
  • 8 replies
  • 0 kudos

serial communication with MATLAB

Posted on December 05, 2013 at 11:42hi! I'm using an STM32F103 micro.I wanna send some data from MATLAB to micro. I'm using ''Keil'' for programming micro. I was wandering whether it is possible to use ''scanf'' in Keil in order to receive data from...