Others: STM32 MCUs related

Find out more about STM32 implementations with external components, discuss use cases, and discover how to use new tools and ST components.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Help with Keil MDK debugger. STM32F072.

I've reinstalled latest Keil MDK v 5.26.2 and have show-stopper issue with debugging STMF072.When the debugger starts, it throws the following error:Load "…………....axf"Error while accessing a target resource. Resource perhaps not available or a wrong ...

Pavel A. by Super User
  • 4879 Views
  • 12 replies
  • 0 kudos

how to set and reset the Option Byte while flash via dual boot option on stm32l476rg along with using mbed os-version 5.x?

Hello,I have done with flash via dual boot option on a STM32L476RG board using an external board NUCLEO- L476. when I am trying to change the option bit via program in which i am using HAL_FLASHEx_OBGetConfig and HAL_FLASHEx_OBProgram. eventually i a...

Ngaur by Associate
  • 713 Views
  • 0 replies
  • 0 kudos

Has anybody tried using CubeMx v5.0.1, Windows 10, STM32 embedded target for MATLAB® and Simulink® release 4.4.2 and Matlab 2016b in their code generation examples?

I have tried using the examples to generate the code , but it seems it does not create an MDK-ARM project. I only see the Matlab generated files but no MDK-ARM project which I can flash directly to the device.I was previously using Matlab 2015b, Wind...

jessica by Associate II
  • 1024 Views
  • 3 replies
  • 1 kudos