cancel
Showing results for 
Search instead for 
Did you mean: 

uPSD3354DV-40U6 Rev.C ?

hg_chen
Associate II
Posted on October 31, 2008 at 05:15

uPSD3354DV-40U6 Rev.C ?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
hg_chen
Associate II
Posted on May 17, 2011 at 11:52

please refer to web site below

http://www.keil.com/support/docs/2795.htm

so is uPSD3354DV-40U6 Rev.C available?

SYMPTOM

In projects using the ST uPSD33xx series devices, the µVision Debugger may fail to halt on breakpoints.

CAUSE

There are a few things that could cause this condition.

The ST PSDsoft utility controls the memory mapping of the device. If this mapping does not concur with the memory mapping in µVision, the debugger will ''get lost'' and won't be able to find the correct locations to place the breakpoints.

There is a problem in the pipeline gates of the Rev-A silicon of the uPSD33xx devices.

RESOLUTION

Compare the memory layout in your PSDsoft project, with your µVision project. Make sure the beginning of CODE space corresponds with the beginning of the executable area on the uPSD device.

Contact ST and ask to upgrade to the Rev-C version of your device