cancel
Showing results for 
Search instead for 
Did you mean: 

SPC582B-DIS with the VNF1248 Evaluation board GUI

Francois_M
Visitor

Dear ST Community,
I recently bought the SPC582B-DIS board in order to test the EV-VNF1248F board. 
I installed the VNF1248 Evaluation board GUI and the UDE STK 2021 by following VNF user guide.
I downloaded the Chorus1M_VNF1248_discovery.elf in order to test the board, I flashed it with this elf file (flash success) but communication is not possible in the GUI with the good COM port  and good serial configuration (error "Cannot found Demo Board! Check USB cable"  in USB FTDI, and no Rx trame in Serial Port)
I tried with another computer, same results. I looked in the forum, I have the good PLS driver (Driver USB PLS\JtagUsbDriver), and I installed the stsw-link009, but still not working.
I also found another elf file on st community website --> Chorus1M_M09SpiDriver.elf, and with this .elf, I'm able to communicate, I get Rx trame and uC is active, but I get the error "firmware is not fitting with HW type", which seems logical.

If I'm not wrong, I (and another post on the same subject) suppose that the Chorus1M_VNF1248_discovery.elf is not working on the SPC582-DIS, but only with the EV-SPC582B which seems to be the old board, and which is out of stock on every distributor.
Would it be possible to generate a .elf which can be compatible with SPC582-DIS to control the VNF1248F? Or to find a solution to my problem ?
@zambrano.luigi@Erwan YVIN@Max VIZZINI, I see that you helped other community member on the subject, could be great if you or another ST member could help me :) 

Thank you a lot.
François 

0 REPLIES 0