2025-09-28 10:57 AM - edited 2025-09-28 11:01 AM
Dear All,
can someone, please, specify the meaning of the bit 1 as 'A8' in the I2C address of the M24C04-FMH6TG?
I can't find any explanation of this value.
Thank you
Solved! Go to Solution.
2025-09-29 12:39 AM
The M24C04 contains 512 (2^9) bytes, which require 9 bits for addressing. Since an address byte only has 8 bits (A0...A7), the 9th bit (A8) must also be transferred, for which bit b1 in the device select code is used.
Does it answer your question?
Regards
/Peter
2025-09-29 12:39 AM
The M24C04 contains 512 (2^9) bytes, which require 9 bits for addressing. Since an address byte only has 8 bits (A0...A7), the 9th bit (A8) must also be transferred, for which bit b1 in the device select code is used.
Does it answer your question?
Regards
/Peter
2025-10-01 3:03 AM
Of course, thanks :D.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.