Skip to main content
Associate
January 7, 2026
Question

Benchmark Validation in App does not match Arduino Uno R4 WiFi

Hello.

Forgive me for what might be an incredibly "noob" question, but i'm not ashamed to admit that I am, in fact, a noob.

I've been trying and failing and trying and moderately succeeding over the last few days using NanoEdge AI Studio creating an audio classification model.

I'm using an Arduino Uno R4 Wifi.  I also have a MAX4466 connected to A0, GND, and 3.3v

My entire process up until now.
1. Get a sketch running on my arduino which simply does a micValue = analogRead(A0) in a loop for 1024 times.  For each read, i so a Serial.print(micValue); Serial.print(" ").  After 1024 of those, I do a Serial.println("") to go to the next line.

2. With that running on the Arduino, I opened NanoEdge Studio, created my project, recorded a bunch of signals of background_noise, silence, me speaking and another sound that i want to classify.  It's not a HUGE dataset, only a couple of minutes, but i'm increasingly adding more to each Class.

3. I ran the benchmark.

4. The benchmark produced some results in the 90+% range.

5. I performed the validation step with me speaking, some background noise, silence, and the beep and it produced a mostly accurate prediction based on what sound i was currently forcing.  When i wasn't speaking, SILENCE was the  most probable.  When I was speaking, SPEECH was the most probably, when i did some shuffling and other stuff background_noise was the most probable and when i played the other sound, that was the most probable.

6. I "deployed" the library (and saved it to my computer)

I added the library in Arduino and can include NanoEdgeAI.h and knowledge.h fine.

I copied this code from the example file.

float input_user_buffer[DATA_INPUT_USER * AXIS_NUMBER]; // Buffer of input values
float output_class_buffer[CLASS_NUMBER]; // Buffer of class probabilities
uint16_t id_class = 0;
const char *id2class[CLASS_NUMBER + 1] = { // Buffer for mapping class id to class name
	"unknown",
	"speech",
	"silence",
	"braun_infusomat",
	"background_noise",
};

In my loop() i'm executing this code:
 get_microphone_data();

 
 neai_classification(input_user_buffer, output_class_buffer, &id_class);
 Serial.print(id_class);
 Serial.print(": ");
 Serial.println(id2class[id_class]);

 for(int x =0; x <= CLASS_NUMBER; x++)
 {
 Serial.println( output_class_buffer[x]);
 }

 delay(100);

However, the results are nowhere near the accuracy of the test performed on the validation tab in NanoEdgeAI Studio.

 

Any thoughts on what i might be doing wrong?

 

4 replies

edwards09Author
Associate
January 7, 2026

Sorry, I also meant to note that i don't move the board OR the microphone when going from emulator to on device.

 

Peter BENSCH
ST Technical Moderator
January 7, 2026

Welcome @edwards09, to the community!

I would like to point out that NanoEdge AI Studio only generates code for Cortex-M based MCUs, but your Uno R4 Wifi is equipped with an ESP32-S3  that has an XTensa LX7 core. Therefore, you cannot use NanoEdge AI Studio for your board. Please also see community threads like this one.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
January 7, 2026

@Peter BENSCH wrote:

NanoEdge AI Studio only generates code for Cortex-M based MCUs, but your Uno R4 Wifi is equipped with an ESP32-S3


The main processor is the Renesas RA4M1 - which is Cortex-M4.

The ESP32 is a "coprocessor" for the WiFi.

 

@edwards09  But still, expecting ST to support a non-ST target is unrealistic.

You need to go to Arduino for support; eg,

https://docs.arduino.cc/tutorials/nano-33-ble-sense/get-started-with-machine-learning/

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
January 8, 2026
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.