Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

New STM32 VSCode extension V2.0.0 released

Changelog Version 2.0.0 V2.0.0 implies a breaking change: CMake project generation has been moved from VS Code to STM32CubeMX v6.11.0 (and later). VS Code solution no longer has dependency on STM32CubeIDE (.cproject-files)VS Code solution no longer r...

VSCode How to install VCPKG on VSCode with Zscaler/Proxy

Issue:  The VSCode don't have the ability to route the extension network requests to the proxy (only VSCode application network is routed to the proxy) I -  the clean way (applies to network with Zscaler installed) ask for a Zscaler power user profil...

NawresGHARBI_1-1704443433898.png NawresGHARBI_2-1704443503313.png NawresGHARBI_3-1704443553581.png NawresGHARBI_4-1704443616206.png

Plot a buffer for signal processing

Hello, I'm doing a project for speech recognition. I have a buffer of 512 values and I want to test every state of the ASR I'm implementing. I am using Keil ARM as IDE and I have tried to use ​the logic analyzer to plot my buffer but I can only plot ...

PTsou.1 by Associate
  • 197 Views
  • 2 replies
  • 0 kudos

printf() in IAR 9.20.2 doesn't work

I have been using prinf() function in IAR 9.10.1 without any issue.  Recently I upgraded to IAR 9.20.2 but the printf() didn't work any more.I also contacted IAR and they said fputc() based printf is not supported by IAR 9.20 any more and recommended...

0693W00000KZjbbQAD.png 0693W00000KZjbgQAD.png 0693W00000KZjbqQAD.png
CKang.3 by Associate
  • 872 Views
  • 1 replies
  • 0 kudos

I am using STM32 Matlab target. In the demo of PIL after completing all the processes and generating code. When I return to Simulink and click continue I got the following error.

The timeout of 5 seconds for receiving data from the rtiostream interface has been exceeded. There might be multiple reasons for this failure.You should: (a) Check that the target hardware configuration is correct, for example, check that the byte or...

UKshi.1 by Associate
  • 165 Views
  • 0 replies
  • 0 kudos

STM32 QSPI works with compiler Version 5 but not 6

I'm not sure if it's more appropriate to post this in the ARM/Keil forum or the STM32 forum so I'm trying both.We have a project based on an STM32F730V8Tx and I need to use the QSPI block. We created a simple test project that just initializes the ex...

EGers by Associate
  • 172 Views
  • 0 replies
  • 0 kudos

Resolved! ST-MCU-FINDER-PC v4.0 does not install on MacOS M1

The SetupSTMCUFinder-4.0.0-RC3 file can be clicked, and it seems like my OS tries to open / run it, but ultimately nothing happens. I remember having a similar issue with another piece of stm software, and remember running some command in the termina...