Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

New STM32 VSCode extension V2.0.0 released

Changelog Version 2.0.0 V2.0.0 implies a breaking change: CMake project generation has been moved from VS Code to STM32CubeMX v6.11.0 (and later). VS Code solution no longer has dependency on STM32CubeIDE (.cproject-files)VS Code solution no longer r...

VSCode How to install VCPKG on VSCode with Zscaler/Proxy

Issue:  The VSCode don't have the ability to route the extension network requests to the proxy (only VSCode application network is routed to the proxy) I -  the clean way (applies to network with Zscaler installed) ask for a Zscaler power user profil...

NawresGHARBI_1-1704443433898.png NawresGHARBI_2-1704443503313.png NawresGHARBI_3-1704443553581.png NawresGHARBI_4-1704443616206.png

Which files to use? CMSIS from Keil of ST?

Posted on June 08, 2012 at 10:31I would like to apologize if this topic is already been discussed, but my search just wasted time.We are trying to figure out which files to use for our ST device (STM32F2xx).We would like to use the ST standard perip...

cameronm by Associate
  • 298 Views
  • 5 replies
  • 0 kudos

USB-FS-Device development kit demo won't compile

Posted on March 27, 2012 at 17:50Has anyone got this to compile.I downloaded it and selected the virtual comport demo.  Compiled it for STM32L152-EVAL board using IAR tools and there are 143 errors.  core_cm3.c '' core does not support this register...

Atollic Toolchain Bug ?

Posted on March 14, 2012 at 16:22I had a strange problem with the Atollic TruStudio Lite toolchain, V2.2. In my project, I had the USART receiving data in the interrupt handler into a buffer, and a main thread evaluating this data, called from main....

Demo: FreeRTOS on STM32F4 Discovery

Posted on January 08, 2012 at 22:58For all interested, I developed a free demo download.  The demo is a simple project which can be dropped into TrueSTUDIO.  Within a few minutes you should be able to have a full blown preemptive real-time operating...

Getting start with Atollic

Posted on February 02, 2012 at 10:16I've just installed Atollic true studio 2.3.0 free edition for ST32 but I don't understand how to setup the IDE with the demo projects of the AN3268. It seems the AN3268 workspace was intended for an older version...

Getting start with IAR 6.30

Posted on February 14, 2012 at 15:27I'm trying the IAR EW6.30 to get start with STM32VL discover board. Following the pdf in the ''stm32vldiscovery_package'' folder, trying to run the demo project of the AN3268, I open the workspace in that folder: ...

Atollic Library Problems

Posted on January 23, 2012 at 03:24Hi all,I am trying to use the arm_cortexM4lf_math.lib in one of my projects, but the linker cannot find it. I have tried just about everything (setting library / library paths etc), but I am a bit new to ST/ARM/Ato...

oli2 by Associate II
  • 294 Views
  • 3 replies
  • 0 kudos

Change clock rate I2C

Posted on January 18, 2012 at 12:13How I can change clock rate for I2C bus? I need to get work wii motion plus. Code from arduino:TWBR = ((16000000L / 400000L) - 16) / 2; // change the I2C clock rateHow I can do this in stm32?I'm use stm32f103vet6. ...

STM32L EEPROM HARD WRITING

Posted on December 23, 2011 at 07:33Good day! The controller has a built-in EEPROM, which is very easy to program by software. It don't suit me. Can I program it during pouring code via the programmer(JLink)? I use Keil4.21 #eeprom #jlink #keil

fiim by Associate III
  • 238 Views
  • 2 replies
  • 0 kudos