Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

New STM32 VSCode extension V2.0.0 released

Changelog Version 2.0.0 V2.0.0 implies a breaking change: CMake project generation has been moved from VS Code to STM32CubeMX v6.11.0 (and later). VS Code solution no longer has dependency on STM32CubeIDE (.cproject-files)VS Code solution no longer r...

VSCode How to install VCPKG on VSCode with Zscaler/Proxy

Issue:  The VSCode don't have the ability to route the extension network requests to the proxy (only VSCode application network is routed to the proxy) I -  the clean way (applies to network with Zscaler installed) ask for a Zscaler power user profil...

NawresGHARBI_1-1704443433898.png NawresGHARBI_2-1704443503313.png NawresGHARBI_3-1704443553581.png NawresGHARBI_4-1704443616206.png

STM32 installer for Windows 11

I'm setting up a new computer. I tried to download STM32 installer for windows 11 from this page https://www.openstm32.org/Downloading%2Bthe%2BSystem%2BWorkbench%2Bfor%2BSTM32%2Binstaller, but it kept saying install_sw4stm32_win_64bits-v2.9.exe canno...

LKa.1 by Associate
  • 1457 Views
  • 0 replies
  • 0 kudos

Toolchains for STM32

Hi. I am a little bit confused.Why there is so many toolchains for ARM and what are the differences betwen them?Lastly i heard abot Yagarto, and also these is WinARM, arm-gcc, arm-none-eabi-gcc. Are they all the same? which toolchain should i use?I a...

sholojda by Associate III
  • 6650 Views
  • 25 replies
  • 0 kudos

Linker Command-line Options not recognized with

I'm migrating from Keil uVision to VS Code, where I provide my own set-up of build flags for ARMCC toolchain. The version of tools I'm using for building my application are the following:I'm trying to use certain linker options that would allow me to...

_legacyfs_online_stmicro_images_0693W00000bkpuy.png
lgacnik97 by Associate III
  • 367 Views
  • 2 replies
  • 0 kudos

Resolved! Need Help with Include paths in Keil compiler

Using Keil V5, C program for stm32g0. Have tried to add include paths in Project.Options for target. C tab. include paths, for instance:C:/Users/ashto/STM32Cube/Repository/STM32Cube_FW_G0_V1.6.1/Drivers/CMSIS/Include;..\..\STM32Cube\Repository\STM32C...

DRobe.4 by Senior
  • 1271 Views
  • 23 replies
  • 0 kudos

HAL i2c & SPI initialization help needed

Hi.I'm using PlatformIO with stm32duino with a NUCLEO-L476RG. I finally figured out how to configure the clocks in CubeMX and then copy the "void SystemClock_Config(void)" function into my main.cpp code and it seems to work great.One question I have ...

YGagn.1 by Associate
  • 261 Views
  • 1 replies
  • 0 kudos